GAPRole Task

The GAPRole task is a separate task which offloads handling most of the GAP layer functionality from the application. This task is enabled and configured by the application during initialization. Based on this configuration, many Bluetooth Low Energy protocol stack events are handled directly by the GAPRole task and never passed to the application. Callbacks exist that the application can register with the GAPRole task so that the application task can be notified of certain events and proceed accordingly.

Based on the configuration of the device, the GAP layer always operates in one of four roles:

  • Broadcaster - The device is an advertiser that is non connectable.
  • Observer - The device scans for advertisements but cannot initiate connections.
  • Peripheral - The device is an advertiser that is connectable and operates as slave in a single link-layer connection.
  • Central - The device scans for advertisements and initiates connections and operates as a master in a single or multiple link-layer connections. The Bluetooth Low Energy central protocol stack supports up to three simultaneous connections.

The Bluetooth Core Specification Version 5.1 allows for certain combinations of multiple-roles, which are supported by the Bluetooth Low Energy protocol stack. For configuration of the Bluetooth low energy stack features, see Developing a Custom Application

For supported GAPRole API, see BLE Stack API Reference.

Peripheral Role

The peripheral GAPRole task is defined in peripheral.c and peripheral.h. See the BLE Stack API Reference for the full API Peripheral Role API including commands, configurable parameters, events, and callbacks. The steps to use this module are as follows:

  1. Initialize the GAPRole parameters. This initialization should occur in the application initialization function. (for example simple_peripheral_init shown in Listing 47.).
Listing 47. Setup of GAP Peripheral Role
 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
 // Setup the GAP Peripheral Role Profile

 {

    uint8_t initialAdvertEnable = TRUE;

    uint16_t advertOffTime = 0;

    uint8_t enableUpdateRequest = DEFAULT_ENABLE_UPDATE_REQUEST;
    uint16_t desiredMinInterval = DEFAULT_DESIRED_MIN_CONN_INTERVAL;
    uint16_t desiredMaxInterval = DEFAULT_DESIRED_MAX_CONN_INTERVAL;
    uint16_t desiredSlaveLatency = DEFAULT_DESIRED_SLAVE_LATENCY;
    uint16_t desiredConnTimeout = DEFAULT_DESIRED_CONN_TIMEOUT;

    // Set the GAP Role Parameters

    GAPRole_setParameter(GAPROLE_ADVERT_ENABLED, sizeof(uint8_t),
    &initialAdvertEnable);
    GAPRole_setParameter(GAPROLE_ADVERT_OFF_TIME, sizeof(uint16_t),
    &advertOffTime); GAPRole_setParameter(GAPROLE_SCAN_RSP_DATA,
    sizeof(scanRspData), scanRspData);
    GAPRole_setParameter(GAPROLE_ADVERT_DATA, sizeof(advertData),
    advertData); GAPRole_setParameter(GAPROLE_PARAM_UPDATE_ENABLE,
    sizeof(uint8_t), &enableUpdateRequest);
    GAPRole_setParameter(GAPROLE_MIN_CONN_INTERVAL,
    sizeof(uint16_t), &desiredMinInterval);
    GAPRole_setParameter(GAPROLE_MAX_CONN_INTERVAL,
    sizeof(uint16_t), &desiredMaxInterval);
    GAPRole_setParameter(GAPROLE_SLAVE_LATENCY, sizeof(uint16_t),
    &desiredSlaveLatency);
    GAPRole_setParameter(GAPROLE_TIMEOUT_MULTIPLIER,
    sizeof(uint16_t), &desiredConnTimeout);
 }
  1. Initialize the GAPRole task and pass application callback functions to GAPRole. This should also occur in the application initialization function.
Listing 48. Registering Callbacks and Initialization.
1
2
 // Start the Device
 VOID GAPRole_StartDevice(&SimpleBLEPeripheral_gapRoleCBs);
  1. Send GAPRole commands from the application. Figure 43. is an example of the application using GAPRole_TerminateConnection().
Listing 49. Terminating Connection
1
 GAPRole_TerminateConnection();

@startuml
participant Application
participant "GAPRole (peripheral.c)" as GAPRole
participant "BLE Stack"


  Application -> GAPRole : GAPRole_TerminateConnection()

group Device not connected
  GAPRole -> Application : return(bleIncorrectMode)
end

group Connected to a device

  GAPRole -> "BLE Stack" : GAP_TerminateLinkReq()

  rnote over "BLE Stack"
   BLE stack attempts to
   terminate the connection
  end note

  "BLE Stack" -> GAPRole : return(status)
  GAPRole -> Application : return(status)


group status==SUCCESS
...
...Link is terminated by the BLE Stack...
...
"BLE Stack" -> GAPRole: Message {LINK_TERMINATED}
"BLE Stack" -> GAPRole: gapRole_processStackMsg
GAPRole->GAPRole : gapRole_processGAPMsg

  rnote over "GAPRole"
  GAP_LINK_TERMINATED_EVENT
  end note

GAPRole-> Application : SimpleBLEPeripheral_stateChangeCB

Application-> Application : SimpleBLEPeripheral_processAppMsg
  rnote over "Application"
  SBP_STATE_CHANGE_EVT
  end note

Application-> Application : SimpleBLEPeripheral_processStateChangeEvt
  rnote over "Application"
  GAPROLE_WAITING
  end note
end

end

@enduml

Figure 43. Context Diagram of Application using GAPRole_TerminateConnection().

Note

The return value only indicates whether the attempt to terminate the connection initiated successfully. The actual termination of connection event is returned asynchronously and is passed to the application through a callback.

  1. The GAPRole task processes most of the GAP-related events passed to it from the Bluetooth Low Energy protocol stack. The GAPRole task also forwards some events to the application. When a link is terminated, the GAPRole automatically restarts advertising. The following code snippet can be found in peripheral.c
Listing 50. Advertising restart upon disconnect
 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
  case GAP_LINK_TERMINATED_EVENT:
    {
      //.......
      //.......
      //.......

      // If device was advertising when connection dropped
      if (gapRole_AdvNonConnEnabled)
      {
        // Continue advertising.
        gapRole_state = GAPROLE_ADVERTISING_NONCONN;
      }
      // Else go to WAITING state.
      else
      {
        if(pPkt->reason == LL_SUPERVISION_TIMEOUT_TERM)
        {
          gapRole_state = GAPROLE_WAITING_AFTER_TIMEOUT;
        }
        else
        {
          gapRole_state = GAPROLE_WAITING;
        }

        // Start advertising, if enabled.
        gapRole_setEvent(START_ADVERTISING_EVT);
      }
    }
    break;

Central Role

The central GAPRole task is defined in central.c and central.h. See the BLE Stack API Reference for the full Central Role API including commands, configurable parameters, events, and callbacks. See the simple_central example project for an example of implementing the central GAPRole. The steps to use this module are as follows.

  1. Initialize the GAPRole parameters. This initialization should occur in the application initialization function (for example in SimpleBLECentral_init). GAP parameters can also be set in this initialization function.
// Setup Central Profile
{
   uint8_t scanRes = DEFAULT_MAX_SCAN_RES;

   GAPCentralRole_SetParameter(GAPCENTRALROLE_MAX_SCAN_RES,
   sizeof(uint8_t), &scanRes);
}
  1. Start the GAPRole task. This involves passing function pointers to application callback function to the central GAPRole. This should also occur in the application initialization function.
VOID GAPCentralRole_StartDevice(&SimpleBLECentral_roleCB);
  1. Send GAPRole commands from the application. Figure 44. is an example of the application using GAPCentralRole_StartDiscovery().

The return status from the protocol stack indicates only whether or not the attempt to perform device discovery was initiated. The actual device discovered is returned asynchronously as a GAP_DEVICE_INFO_EVENT forwarded through the central GAPRole callbacks as described below.

  1. The GAPRole task performs some processing on the GAP events it receives from the protocol stack. The task also forwards some events to the application. Figure 44. also shows how the GAP_DEVICE_INFO_EVENT is processed from the protocol stack to the application.

@startuml
participant Application
participant "GAPRole (central.c)" as GAPRole
participant "BLE Stack"


  Application -> GAPRole : GAPCentralRole_StartDiscovery\n(MODE, ACTIVE_SCAN, WHITE_LIST)

group scanning || ! (central or observer)
  GAPRole -> Application : return(bleIncorrectMode)
end

group !scanning && (central or observer)

  GAPRole -> "BLE Stack" : GAP_DeviceDiscoveryRequest()

  rnote over "BLE Stack"
   BLE stack attempts to
   start device discovery
  end note

  "BLE Stack" -> GAPRole : return(status)
  GAPRole -> Application : return(status)


group status==SUCCESS
...
... BLE Stack does device discovery ...
...
"BLE Stack" -> GAPRole: Message {DISCOVERY_DONE}
"BLE Stack" -> GAPRole: gapCentralRole_processStackMsg
GAPRole->GAPRole : gapCentralRole_ProcessGAPMsg
GAPRole->Application: SimpleBLECentral_eventCB
Application ->Application: SimpleBLECentral_processStackMsg
Application ->Application: SimpleBLECentral_processRoleEvent

  rnote over "Application"
  GAP_DEVICE_DISCOVERY_EVENT
  end note
end

end

@enduml

Figure 44. Context Diagram of Application using GAPCentralRole_StartDiscovery().

Note that during scanning, as defined by the Bluetooth Core Specification Version 5.1, individual advertisements / scan responses are returned as GAP_DEVICE_INFO_EVENT. By default, duplicate reports are filtered such that only one event is returned to the application per unique address and data pair. This can be configured via the TGAP_FILTER_ADV_REPORTS GAP parameter. After the scan has completed, a summary of discovered reports will be returned to the application as a GAP_DEVICE_DISCOVERY_EVENT.

The maximum amount of scan responses that can be discovered during one scan can be set with the GAPCENTRALROLE_MAX_SCAN_RES parameter. In an environment saturated with advertisements / scan responses, this can have a drastic impact on heap usage to the point of potentially breaking the stack. Therefore, it is essential to profile your application for the worst-case scenario where the maximum amount of scan responses are discovered during a scan.

In the worst-case scenario where the maximum number of advertisements / scan responses ( n ) is found during a scan, all with the maximum data size, in which the application is consistently processing such that it does not process any of the stack’s messages, the heap could grow by: ( 8 + 87 * n bytes ). For example, if GAPCENTRALROLE_MAX_SCAN_RES is set to 10, there must be at least 878 bytes available for allocation from the heap. This includes a completely filled GAP_DEVICE_DISCOVERY_EVENT. If this allocation fails, a GAP_DEVICE_DISCOVERY_EVENT with error status will attempt to be allocated instead which is only 8 bytes. Therefore, in order for the system to keep running in the scenario described above, the heap must have space to allocate at least ( 8 + 79 * n bytes ). See the Debugging chapter for steps to profile the heap.

Initiating a Connection

In order to enter a connection with a device, a connect request must be sent. Usually this is done after scanning completes if the desired device is found, but it is possible to connect directly to a device if its address and address type are known. The API for establishing connections is GAPCentralRole_EstablishLink() for a central role or GAPRole_EstablishLink() for a multi role. Both these APIs simply fill out the proper structure and call GAP_EstablishLinkReq().

Initiating a connection is a combined operation, it consists of

  1. Scanning for the device
  2. Send a connect request (if a device is found)

If the device is not found, then the link layer will continue to scan indefinitely. Attempting to establish an additional connection while initiating is in progress will return the error bleAlreadyInRequestedMode.

There exists a condition where the advertising device may be detected during general scanning (i.e. found via GAP_DEVICE_INFO_EVENT), but may not be detected during the connection initiation scan. (e.g. user walked away, or battery died). For this reason it maybe desirable to create a timeout for initiating in the application. The initiating connection task in the link layer can be stopped with: GAPCentralRole_TerminateLink() or GAPRole_TerminateConnection() with connection handle set to GAP_CONNHANDLE_INIT.