Application Layer

Since the micro stack can support multiple functionalities (broadcaster, observer, connection monitor), it is up to the application layer to define the behavior of the system. The following sections will discuss the TI provided implementations of the broadcaster and monitor roles.

  • micro_ble_cm.c : Connection monitor application
  • micro_eddystone_beacon.c : Broadcaster application implementing the Eddystone protocol

Connection Monitor (CM) Application

The connection monitor application is built on top of the uGAP layer operating in monitor mode and is responsible for implementing the high level connection tracking feature. This includes:

  1. Initializing connection parameters for a connection to monitor
  2. Performing the initial scan to find a connection event
  3. Scheduling subsequent scans to continue following the connection

The following sections will describe the above list in detail.

Initializing CM Session

In order to follow a connection, the CM needs to know the connection parameters that were exchanged during the connection process between master and slave. These include:

  • access address
  • connection interval
  • hop value
  • next channel
  • channel map
  • CRC initialization value

These parameters can be obtained from a BLE(5)-Stack application by calling the HCI_EXT_GetActiveConnInfoCmd command. Once they are obtained, they should be shared (via an out of band mechanism such as UART, LIN, CAN etc) with the CM device. The CM device then can use ubCM_startExt() to start the initial scan.

Starting a Monitor Session

In order to start tracking a connection the connection monitor needs to perform an initial wide scan in order to catch a connection event. This scan should be at worst case the connection interval times the number of active channels in order to ensure the connection can be detected.

The logic trace below was generated by enabling the RF observable pins on master and slave device in the connection (RX, TX) as well as the connection monitor (RX). It shows the initial scan.

../_images/cm-initial-scan.png

Following a connection

Once a packet is received during the initial scan the CM will setup smaller scans based on the next expected event. Since it is now following the connection, it can calculate the channel and instant (adjusted for master and slave sleep clock accuracy) to listen for the next event.

The core of connection following is based on

  • monitor_indicationCB : Invoked when a packet is received
  • monitor_completeCB : Invoked when a scan window has completed.

The logic trace below shows the CM actively tracking a connection

../_images/cm-conn.png

Micro Eddystone Beacon App

Note

The Micro Eddyston Beacon app is not available in all SDKs such as CC26x2/CC13x2. It can be found in the CC2640R2 SDK.

The Micro Eddystone Beacon app implements the Google Eddystone. Protocol. The details of the protocol are outside the scope of this document. Instead, this section will focus on the primary elements of the broadcaster role.

The key parts of the broadcaster role includes:

  1. Initializing the device address
  2. Starting and stopping advertising
  3. Processing the change of advertising data
  4. Consuming the uGAP broadcast callbacks

Device Address

The micro stack will use a the public address that is burned into the device. A static address can be used if FEATURE_STATIC_ADDR is defined.

The micro-stack will be initialized with the device address using uble_stackInit().

Start/Stop Advertising

The application will control the start and stop of advertising based on button press. Starting advertisement involves setting the TX power and calling ugap_bcastStart()

Changing Advertising data

The advertisement data can be changed on the fly with a call to uble_setParameter with the parameter ID UBLE_PARAM_ADVDATA. The beacon will do so as specified by the Eddystone protocol.

Processing Micro GAP Advertising Callbacks

There are three callbacks that are of interest to the broadcaster role

  • ugapBcastStateChangeCb_t : The Micro GAP has changed states
  • ugapBcastAdvPrepareCb_t: The Micro GAP is preparing an advertisement
  • ugapBcastAdvDoneCb_t : The Micro GAP has completed an advertisement

State change

The states of interest to the application are:

  • UGAP_BCAST_STATE_INITIALIZED: The micro stack has been initialized and is ready for commands
  • UGAP_BCAST_STATE_IDLE : The micro stack is idle and not performing any function
  • UGAP_BCAST_STATE_ADVERTISING: The micro stack is actively advertising
  • UGAP_BCAST_STATE_WAITING : The micro stack is idle during an off duty cycle period

Micro Stack Parameters

The micro stack has a small layer that is responsible for setting up the various parameters used across the stack. This is encapsulated in uble.c.

In addition to parameter management, the uble layer defines callbacks, a message format, and event proxy function that is used to build and post events from higher priority context (e.g. RF driver callback) to the micro stack. The uble layer is responsible for address management.

Important uble parameters are described below.

Priority

Micro BLE Stack has an overall stack priority that is applied to every issued radio command. The stack priority is intended to give Micro BLE Stack a relative priority against the other RF clients. The stack priority is saved in RFPriority through uble_setParameter(). UBLE_RF_PRI_NORMAL, UBLE_RF_PRI_HIGH, and UBLE_RF_PRI_HIGHEST are translated into RF_PriorityNormal, RF_PriorityHigh, and RF_PriorityHighest respectively when the Micro BLE Stack calls RF_scheduleCmd().

If Micro BLE Stack’s priority is higher than another RF clients, every Micro BLE Stack’s radio command gets privileged unless the priority of other RF client command which has been scheduled is RF_PriorityHighest.

Note that the priority of strictly time-critical and crucial commands, such as CMD_PROP_RX_ADV for beacon reception in TI-15.4-Stack, tends to be set to RF_PriorityHighest regardless of the stack priority.

Time Critically

Time Criticality is how important a radio command being executed at an exact time is. Time Criticality is saved in RFTimeCriticality through ub_uble_setParam(). For example, if advertising events absolutely cannot be missed, and it is okay for the micro stack to preempt other RF activity, then rfPriority should be set to RF_TIME_CRITICAL. Otherwise, rfPriority should be set to RF_TIME_RELAXED.

Scheduling

When the Micro BLE Stack schedules a command, Priority and Time Criticality are passed to RF_scheduleCmd(). These parameters are contained in the priority element of RF_ScheduleCmdParams and pastTrig field in startTrigger element of the RF driver command struct.

If rfPriority is RF_TIME_CRITICAL so the command has to start at a designated time, a failure returned if the radio is unavailable to schedule the command at the moment requested. RF_scheduleCmd() rejects the command if any portion of the desired time period reserved by the same- or higher-priority operation of other RF clients or the RF driver command queue is full.

If rfPriority is RF_TIME_RELAXED so the command can be delayed if the radio is unavailable at moment requested; that command is scheduled with pastTrig=1. Once the command with pastTrig=1 is scheduled successfully, it will start at the desired start time if the radio is available, or when the radio is available after the start time.

The RF Event RF_EventRadioAvailable needs to be activated since it is used for rescheduling

Micro RF interface

The micro RF interface or urfi is responsible for instantiating and configuring various RF commands used by the micro stack.

The following RF commands are used by the micro stack

  • rfc_CMD_BLE_ADV_COMMON_t : Advertiser command, used by broadcaster
  • rfc_CMD_BLE_SCANNER_t : Scanner command, used by observer
  • rfc_CMD_BLE_GENERIC_RX_t : Generic RX command, used by connection monitor

Micro GAP

The uGAP sits between the uLL and the application and is responsible for controlling the uLL to set up and run profile roles. The application can indirectly configure the uLL through the uGAP and be notified of events from the uLL through uGAP callbacks.

Parameters Management

The uGAP maintains the following parameters that control its behavior

ugbNumAdvEvent

The number of advertising events to be done before the Broadcaster stops its job. This is given when the application starts the Broadcaster by calling ug_bcastStart(). If this parameter is set to 0, the Broadcaster will not go to UGAP_BCAST_STATE_INITIALIZED state once started unless it is requested to stop.

ugbDutyOnTime

Time period during which the Broadcaster stays in UGAP_BCAST_STATE_ADVERTISING state. The uLL stays in Advertising State as well. When this time period ends, the Broadcaster state will transition to UGAP_BCAST_STATE_WAITING and the uLL will exit Advertising State. This parameter is effective only if Broadcaster Duty Control is enabled. If Broadcaster Duty Control is disabled, transition to other state from UGAP_BCAST_STATE_ADVERTISING is not affected by this parameter. A 100-ms time unit is used.

ugbDutyOffTime

Time period during which the Broadcaster stays in UB_BCAST_STATE_WAITING state. The uLL cannot be in Advertising State during this period. When this time period ends, the Broadcaster state will transition to UGAP_BCAST_STATE_ADVERTISING and the uLL will enter Advertising State. This parameter is effective only if Broadcast Duty Control is enabled. If 0, Broadcaster Duty Control is disabled and the Broadcaster will not enter UGAP_BCAST_STATE_WAITING state. A 100-ms time unit is used.

Role Management

The uGAP is the main interface to operate in various roles.

There are two distinct roles the uGAP supports:

  • Broadcaster
  • Monitor

The application must configure the uGAP to operate in the mode desired. This section goes over specifics of the individual roles.

Broadcaster Role

If the application configures the uGAP to operate Broadcaster role, the uGAP lets the uLL send advertising events as described in Advertising State in accordance with the parameters listed in Application Parameters.

The Broadcaster Role has 4 states:

  • UG_BCAST_STATE_INITIALIZED: Broadcaster is initialized but has never started. The corresponding state of the uLL can be anything but ULL_STATE_ADVERTISING.
  • UGAP_BCAST_STATE_ADVERTISING: Broadcaster is advertising in this state. The corresponding state of the uLL is ULL_STATE_ADVERTISING. If Broadcaster Duty Control is enabled, the duty timer starts with the duration of BcastDutyOnTime when this state is entered. Then, the state switches to UGAP_BCAST_STATE_WAITING when the duty timer expires. If 0 was passed to NumAdvEvent when ug_bcastStart() is called, ugbNumAdvEvent won’t have any effect on this state. Otherwise, the state switches to UG_BCAST_STATE_IDLE if requested through ug_bcastStop() or the total number of Advertising Events since ug_bcastStart() was called reaches ugbNumAdvEvent. If ug_bcastSuspend() is called, the state switches to UGAP_BCAST_STATE_SUSPENDED, putting the duty timer on hold if Duty Control is enabled. The duty timer will resume when the state switches back to this state.
  • UGAP_BCAST_STATE_WAITING: Broadcaster started but is not advertising in this state because it’s in DutyOffTime period. The corresponding state of the uLL is UL_STATE_STANDBY. If Broadcaster Duty Control is enabled, the duty timer starts with the duration of BcastDutyOffTime when this state is entered. Then, the state switches to UGAP_BCAST_STATE_ADVERTISING when the duty timer expires. The state switches to UG_BCAST_STATE_IDLE if requested through ug_bcastStop(). If ug_bcastSuspend() is called, the state switches to UGAP_BCAST_STATE_SUSPENDED, putting the duty timer on hold if Duty Control is enabled. The duty timer will resume when the state switches back to this state.
  • UGAP_BCAST_STATE_SUSPENDED: Broadcaster started but is not advertising in this state. The corresponding state of the uLL can be anything but ULL_STATE_ADVERTISING. The former state shall be recorded when this state is entered. If the suspension is lifted through ug_bcastResume(), the state will switch back to the former state. The state switches to UG_BCAST_STATE_IDLE if ug_bcastStop() is called.
alternate text

Figure 80. Broadcaster states

The BLE specification doesn’t allow Broadcaster to have Limited Discoverable Mode. However, the uGAP provides a duty control means similar to Limited Discoverable Mode to save power consumption. The duty control can be implemented with timers based on BcastDutyOnTime and BcastDutyOffTime explained in Parameters Management. Broadcaster’s Advertising State corresponds to the uLL’s Advertising State.

The typical life cycle of the Broadcasting function encompassing the application down to the uLL is illustrated in Figure 81.

alternate text

Figure 81. Life Cycle of Broadcaster Function

Monitor Role

The Monitor Role is not an official BLE Specification role. This section is to describe how the uGAP operates when using the Monitor Feature.

This role is tested in stand alone condition only. No other uBLE Stack feature should be used in conjunction.

Monitor role is designed to follow an active BLE connection if given connection information such as access address, hop increment, and connection interval. With this information the Monitor role sets up uGAP and uBLE.

The Monitor Role has 3 States:

  • UGAP_MONITOR_STATE_INITIALIZED: The monitor is initialized but is not monitoring.
  • UGAP_MONITOR_STATE_IDLE: The monitor is not monitoring in this state. This corresponds to UL_STATE_STANDBY in the uLL.
  • UGAP_MONITOR_STATE_MONITORING: The monitor is scanning. This corresponds to UL_STATE_MONITORING in the uLL.

When a packet is detected with the during a scan with the Connection Parameters passed in from the ‘uble.c’ source file a UGAP_MONITOR_EVT_MONITOR_INDICATION event is generated.

When a scan is complete, a UGAP_MONITOR_EVT_MONITOR_COMPLETE event is generated. If there are pending scans, the uGAP will start the next scheduled scan.

Each time the Monitor switches states, a UGAP_MONITOR_EVT_STATE_CHANGE event is generated.