![]() |
![]() |
|
TI BLE-Stack for Bluetooth API Documentation
3.03.05.00
|
Macros | |
| #define | GAPCENTRALROLE_BD_ADDR 0x403 |
| Device Address read from the controller (Read-only) More... | |
| #define | GAPCENTRALROLE_IRK 0x400 |
| Identity Resolving Key (Read/Write) More... | |
| #define | GAPCENTRALROLE_LINK_PARAM_UPDATE_REQ_REPLY 0x405 |
| Action taken when a parameter update fails (Read/Write) More... | |
| #define | GAPCENTRALROLE_MAX_SCAN_RES 0x404 |
| Maximmum number of scan reports to store from GAPCentralRole_StartDiscovery (Read/Write) More... | |
| #define | GAPCENTRALROLE_SIGNCOUNTER 0x402 |
| Sign Counter (Read/Write) More... | |
| #define | GAPCENTRALROLE_SRK 0x401 |
| Signature Resolving Key (Read/Write) More... | |
Parameters set via GAPCentralRole_SetParameter
| #define GAPCENTRALROLE_BD_ADDR 0x403 |
Device Address read from the controller (Read-only)
The BDADDR is read, in increasing order of priortiy, from the info page, secondary address from flash, or set from HCI_ReadBDADDRCmd
size: uint8_t[6]
default: BDADDR from info page
range: 0x000000000000 - 0xFFFFFFFFFFFE
| #define GAPCENTRALROLE_IRK 0x400 |
Identity Resolving Key (Read/Write)
size: uint8_t[16]
default: 0x00000000000000000000000000000000
range: 0x00000000000000000000000000000000 - 0xFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFIdentity Resolving Key. Read/Write. Size is uint8_t[KEYLEN]. Default is all 0, which means that the IRK will be randomly generated.
| #define GAPCENTRALROLE_LINK_PARAM_UPDATE_REQ_REPLY 0x405 |
Action taken when a parameter update fails (Read/Write)
size: uint8_t[16]
| #define GAPCENTRALROLE_MAX_SCAN_RES 0x404 |
Maximmum number of scan reports to store from GAPCentralRole_StartDiscovery (Read/Write)
size: uint8_t
default: 8
range: 0-256 but this will be constrained by available RAM
| #define GAPCENTRALROLE_SIGNCOUNTER 0x402 |
Sign Counter (Read/Write)
size: uint32_t
default: 0x0000
range: 0x0000 - 0xFFFF
| #define GAPCENTRALROLE_SRK 0x401 |
Signature Resolving Key (Read/Write)
size: uint8_t[16]
default: 0x00000000000000000000000000000000
range: 0x00000000000000000000000000000000 - 0xFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFSignature Resolving Key. Read/Write. Size is uint8_t[KEYLEN]. Default is all 0, which means that the SRK will be randomly generated.