TI BLE-Stack for Bluetooth API Documentation
3.03.05.00
|
Multi GAPRole Callback structure. More...
Data Fields | |
paramUpdateAppDecision_t | pfnParamUpdateAppDecision |
When the app should decide on a param update request. | |
passThroughToApp_t | pfnPassThrough |
When the event should be processed by the app instead of the GAP Role. | |
gapRolesStateNotify_t | pfnStateChange |
Whenever the device changes state. | |
Multi GAPRole Callback structure.
Peripheral GAPRole Callback structure.
This must be setup by the application and passed to the GAPRole when GAPRole_StartDevice is called.