![]() |
![]() |
|
TI BLE5-Stack API Documentation
1.01.13.00
|
Type definitions and macros for BLE stack.
Go to the source code of this file.
Macros | |
| #define | B_ADDR_LEN 6 |
| Default Public and Random Address Length. | |
| #define | B_APP_DEFAULT_PASSCODE 123456 |
| BLE Default Passcode. | |
| #define | B_CHANNEL_MAP_LEN 5 |
| BLE Channel Map length. | |
| #define | B_EVENT_MASK_LEN 8 |
| BLE Event mask length. | |
| #define | B_FEATURE_SUPPORT_LENGTH 8 |
| BLE Feature Supported length. | |
| #define | B_LOCAL_NAME_LEN 248 |
| BLE Local Name length. | |
| #define | B_MAX_ADV_LEN 31 |
| BLE Maximum Advertising Packet Length. | |
| #define | B_RANDOM_NUM_SIZE 8 |
| BLE Random Number Size. | |
| #define | B_RESOLVING_LIST_SIZE 3 |
| BLE Privacy Resolving List Size For Peer Keys. | |
| #define | BLE_LRU_BOND_LIST 0x05 |
| The Device's order of bond indexes in least recently used order. | |
| #define | BLE_NVID_ADDR_MODE 0x04 |
| The Device's address type (GAP_Addr_Modes_t) | |
| #define | BLE_NVID_CSRK 0x03 |
| The Device's CSRK. | |
| #define | BLE_NVID_CUST_END 0x8F |
| End of the Customer's NV IDs. | |
| #define | BLE_NVID_CUST_START 0x80 |
| Start of the Customer's NV IDs. | |
| #define | BLE_NVID_GAP_BOND_END 0x5f |
| End of the GAP Bond Manager's NV IDs Range. | |
| #define | BLE_NVID_GAP_BOND_START 0x20 |
| Start of the GAP Bond Manager's NV IDs. | |
| #define | BLE_NVID_GATT_CFG_END 0x79 |
| End of the GATT Configuration NV IDs. | |
| #define | BLE_NVID_GATT_CFG_START 0x70 |
| Start of the GATT Configuration NV IDs. | |
| #define | BLE_NVID_IRK 0x02 |
| The Device's IRK. | |
| #define | BLE_NVID_RANDOM_ADDR 0x06 |
| The Device's random address if set by the current GAP_DeviceInit. | |
| #define | bleAlreadyInRequestedMode 0x11 |
| Already performing that task. | |
| #define | bleGAPBondRejected 0x32 |
| The bound information was rejected. | |
| #define | bleGAPBufferInUse 0x33 |
| The buffer is in use elsewhere. | |
| #define | bleGAPConnNotAcceptable 0x31 |
| The connection was not accepted. | |
| #define | bleGAPFilteredOut 0x35 |
| The received PDU was filtered out. | |
| #define | bleGAPNotFound 0x34 |
| No handle / buffer found. | |
| #define | bleGAPUserCanceled 0x30 |
| The user canceled the task. | |
| #define | bleIncorrectMode 0x12 |
| Not setup properly to perform that task. | |
| #define | bleInsufficientAuthen 0x41 |
| The attribute has insufficient authentication. | |
| #define | bleInsufficientEncrypt 0x42 |
| The attribute has insufficient encryption. | |
| #define | bleInsufficientKeySize 0x43 |
| The attribute has insufficient encryption key size. | |
| #define | bleInternalError 0x1E |
| Internal error not due to application. | |
| #define | bleInvalidMtuSize 0x1B |
| MTU size is out of range. | |
| #define | bleInvalidPDU 0x40 |
| The attribute PDU is invalid. | |
| #define | bleInvalidRange 0x18 |
| A parameter is out of range. | |
| #define | bleInvalidTaskID INVALID_TASK |
| Task ID isn't setup properly. | |
| #define | bleLinkEncrypted 0x19 |
| The link is already encrypted. | |
| #define | bleMemAllocError 0x13 |
| Memory allocation error occurred. | |
| #define | bleMemFreeError 0x1D |
| Memory free error occurred. | |
| #define | bleNoResources 0x15 |
| There are no resource available. | |
| #define | bleNotConnected 0x14 |
| Can't perform function when not in a connection. | |
| #define | bleNotReady 0x10 |
| Not ready to perform task. | |
| #define | blePairingTimedOut 0x1C |
| Previous pairing attempt timed out. | |
| #define | blePending 0x16 |
| Waiting. | |
| #define | bleProcedureComplete 0x1A |
| The Procedure is completed. | |
| #define | bleTimeout 0x17 |
| Timed out performing function. | |
| #define | DISPATCH_CMD_EVENT 0x82 |
| Dispatch Command Event message. | |
| #define | GAP_EVENT_SIGN_COUNTER_CHANGED 0x4000 |
| The device level sign counter changed. | |
| #define | GAP_MSG_EVENT 0xD0 |
| Incoming GAP message. | |
| #define | GATT_MSG_EVENT 0xB0 |
| Incoming GATT message. | |
| #define | GATT_SERV_MSG_EVENT 0xB1 |
| Incoming GATT Serv App message. | |
| #define | HCI_DATA_EVENT 0x90 |
| HCI Data Event message. | |
| #define | HCI_EXT_CMD_EVENT 0x93 |
| HCI Extended Command Event message. | |
| #define | HCI_GAP_EVENT_EVENT 0x91 |
| GAP Event message. | |
| #define | HCI_GAP_META_EVENT_EVENT 0x95 |
| GAP Meta Event message. | |
| #define | HCI_SMP_EVENT_EVENT 0x92 |
| SMP Event message. | |
| #define | HCI_SMP_META_EVENT_EVENT 0x94 |
| SMP Meta Event message. | |
| #define | ICALL_CMD_EVENT 0x81 |
| ICall Command Event message. | |
| #define | ICALL_EVENT_EVENT 0x80 |
| ICall Event message. | |
| #define | INVALID_TASK_ID 0xFF |
| Task ID isn't setup properly. | |
| #define | KEYLEN 16 |
| Default key length. | |
| #define | L2CAP_DATA_EVENT 0xA0 |
| Incoming data on a channel. | |
| #define | L2CAP_SIGNAL_EVENT 0xA2 |
| Incoming Signaling message. | |
| #define | LSB_2_BYTES 2 |
| #define | MSB_4_BYTES 4 |
| 4 BYTES MSB | |
| #define | SM_MSG_EVENT 0xC2 |
| Incoming SM message. | |
| #define | SM_NEW_RAND_KEY_EVENT 0xC1 |
| New Rand Key Event message. | |
| #define | TI_BASE_UUID_128(uuid) |
| TI Base 128-bit UUID: F000XXXX-0451-4000-B000-000000000000. More... | |
Typedefs | |
| typedef Status_t | bStatus_t |
| BLE Generic Status return. | |
| #define LSB_2_BYTES 2 |
Defines for decomposed Address 2 BYTES LSB
| #define TI_BASE_UUID_128 | ( | uuid | ) |
TI Base 128-bit UUID: F000XXXX-0451-4000-B000-000000000000.