TI BLE5-Stack API Documentation
1.01.13.00
|
GAP layer interface.
Go to the source code of this file.
Data Structures | |
struct | Gap_ConnEventRpt_t |
struct | gapAuthCompleteEvent_t |
struct | gapAuthParams_t |
struct | gapBondCompleteEvent_t |
struct | gapBondMgrCBs_t |
Callback Registration Structure. More... | |
struct | gapDeviceInitDoneEvent_t |
struct | gapEstLinkReqEvent_t |
struct | gapEventHdr_t |
GAP event header format. More... | |
struct | gapLinkUpdateEvent_t |
struct | gapPairingReq_t |
struct | gapPairingReqEvent_t |
struct | gapPasskeyNeededEvent_t |
struct | gapPeriConnectParams_t |
struct | gapSignUpdateEvent_t |
struct | gapSlaveSecurityReqEvent_t |
struct | gapTerminateLinkEvent_t |
struct | gapUpdateLinkParamReq_t |
struct | gapUpdateLinkParamReqEvent_t |
GAP_UPDATE_LINK_PARAM_REQ_EVENT message format. More... | |
struct | gapUpdateLinkParamReqReply_t |
Macros | |
#define | GAP_ADTYPE_128BIT_COMPLETE 0x07 |
Service: Complete list of 128-bit UUIDs. | |
#define | GAP_ADTYPE_128BIT_MORE 0x06 |
Service: More 128-bit UUIDs available. | |
#define | GAP_ADTYPE_16BIT_COMPLETE 0x03 |
Service: Complete list of 16-bit UUIDs. | |
#define | GAP_ADTYPE_16BIT_MORE 0x02 |
Service: More 16-bit UUIDs available. | |
#define | GAP_ADTYPE_32BIT_COMPLETE 0x05 |
Service: Complete list of 32-bit UUIDs. | |
#define | GAP_ADTYPE_32BIT_MORE 0x04 |
Service: More 32-bit UUIDs available. | |
#define | GAP_ADTYPE_3D_INFO_DATA 0x3D |
3D Information Data | |
#define | GAP_ADTYPE_ADV_INTERVAL 0x1A |
Advertising Interval. | |
#define | GAP_ADTYPE_APPEARANCE 0x19 |
Appearance. | |
#define | GAP_ADTYPE_FLAGS 0x01 |
Gap Advertising Flags. | |
#define | GAP_ADTYPE_FLAGS_BREDR_NOT_SUPPORTED 0x04 |
Discovery Mode: BR/EDR Not Supported. | |
#define | GAP_ADTYPE_FLAGS_GENERAL 0x02 |
Discovery Mode: LE General Discoverable Mode. | |
#define | GAP_ADTYPE_FLAGS_LIMITED 0x01 |
Discovery Mode: LE Limited Discoverable Mode. | |
#define | GAP_ADTYPE_LE_BD_ADDR 0x1B |
LE Bluetooth Device Address. | |
#define | GAP_ADTYPE_LE_ROLE 0x1C |
LE Role. | |
#define | GAP_ADTYPE_LOCAL_NAME_COMPLETE 0x09 |
Complete local name. | |
#define | GAP_ADTYPE_LOCAL_NAME_SHORT 0x08 |
Shortened local name. | |
#define | GAP_ADTYPE_MANUFACTURER_SPECIFIC 0xFF |
#define | GAP_ADTYPE_OOB_CLASS_OF_DEVICE 0x0D |
Simple Pairing OOB Tag: Class of device (3 octets) | |
#define | GAP_ADTYPE_OOB_SIMPLE_PAIRING_HASHC 0x0E |
Simple Pairing OOB Tag: Simple Pairing Hash C (16 octets) | |
#define | GAP_ADTYPE_OOB_SIMPLE_PAIRING_RANDR 0x0F |
Simple Pairing OOB Tag: Simple Pairing Randomizer R (16 octets) | |
#define | GAP_ADTYPE_POWER_LEVEL 0x0A |
TX Power Level: 0xXX: -127 to +127 dBm. | |
#define | GAP_ADTYPE_PUBLIC_TARGET_ADDR 0x17 |
Public Target Address. | |
#define | GAP_ADTYPE_RANDOM_TARGET_ADDR 0x18 |
Random Target Address. | |
#define | GAP_ADTYPE_SERVICE_DATA 0x16 |
Service Data - 16-bit UUID. | |
#define | GAP_ADTYPE_SERVICE_DATA_128BIT 0x21 |
Service Data - 128-bit UUID. | |
#define | GAP_ADTYPE_SERVICE_DATA_32BIT 0x20 |
Service Data - 32-bit UUID. | |
#define | GAP_ADTYPE_SERVICES_LIST_128BIT 0x15 |
Service Solicitation: list of 128-bit Service UUIDs. | |
#define | GAP_ADTYPE_SERVICES_LIST_16BIT 0x14 |
Service Solicitation: list of 16-bit Service UUIDs. | |
#define | GAP_ADTYPE_SIGNED_DATA 0x13 |
Signed Data field. | |
#define | GAP_ADTYPE_SIMPLE_PAIRING_HASHC_256 0x1D |
Simple Pairing Hash C-256. | |
#define | GAP_ADTYPE_SIMPLE_PAIRING_RANDR_256 0x1E |
Simple Pairing Randomizer R-256. | |
#define | GAP_ADTYPE_SLAVE_CONN_INTERVAL_RANGE 0x12 |
#define | GAP_ADTYPE_SM_OOB_FLAG 0x11 |
Security Manager OOB Flags. | |
#define | GAP_ADTYPE_SM_TK 0x10 |
Security Manager TK Value. | |
#define | GAP_ADV_REMOVE_SET_EVENT 0x13 |
Sent when an advertising set needs to be removed. This is an internal event. | |
#define | GAP_APPEARE_GENERIC_BARCODE_SCANNER 0x02C0 |
Generic Barcode Scanner. | |
#define | GAP_APPEARE_GENERIC_BLOOD_PRESSURE 0x0380 |
Generic Blood Pressure. | |
#define | GAP_APPEARE_GENERIC_BP_ARM 0x0381 |
Blood Pressure: Arm. | |
#define | GAP_APPEARE_GENERIC_BP_WRIST 0x0382 |
Blood Pressure: Wrist. | |
#define | GAP_APPEARE_GENERIC_CLOCK 0x0100 |
Generic Clock. | |
#define | GAP_APPEARE_GENERIC_COMPUTER 0x0080 |
Generic Computer. | |
#define | GAP_APPEARE_GENERIC_DISPLAY 0x0140 |
Generic Display. | |
#define | GAP_APPEARE_GENERIC_EYE_GALSSES 0x01C0 |
Generic Eye-glasses. | |
#define | GAP_APPEARE_GENERIC_HID 0x03C0 |
Generic Human Interface Device (HID) | |
#define | GAP_APPEARE_GENERIC_HR_SENSOR 0x0340 |
Generic Heart rate Sensor. | |
#define | GAP_APPEARE_GENERIC_HRS_BELT 0x0341 |
Heart Rate Sensor: Heart Rate Belt. | |
#define | GAP_APPEARE_GENERIC_KEYRING 0x0240 |
Generic Keyring. | |
#define | GAP_APPEARE_GENERIC_MEDIA_PLAYER 0x0280 |
Generic Media Player. | |
#define | GAP_APPEARE_GENERIC_PHONE 0x0040 |
Generic Phone. | |
#define | GAP_APPEARE_GENERIC_RC 0x0180 |
Generic Remote Control. | |
#define | GAP_APPEARE_GENERIC_TAG 0x0200 |
Generic Tag. | |
#define | GAP_APPEARE_GENERIC_THERMO_EAR 0x0301 |
Thermometer: Ear. | |
#define | GAP_APPEARE_GENERIC_THERMOMETER 0x0300 |
Generic Thermometer. | |
#define | GAP_APPEARE_GENERIC_WATCH 0x00C0 |
Generic Watch. | |
#define | GAP_APPEARE_HID_BARCODE_SCANNER 0x03C8 |
HID Barcode Scanner. | |
#define | GAP_APPEARE_HID_DIGITAL_CARDREADER 0x03C6 |
HID Card Reader. | |
#define | GAP_APPEARE_HID_DIGITAL_PEN 0x03C7 |
HID Digital Pen. | |
#define | GAP_APPEARE_HID_DIGITIZER_TYABLET 0x03C5 |
HID Digitizer Tablet. | |
#define | GAP_APPEARE_HID_GAMEPAD 0x03C4 |
HID Gamepad. | |
#define | GAP_APPEARE_HID_JOYSTIC 0x03C3 |
HID Joystick. | |
#define | GAP_APPEARE_HID_KEYBOARD 0x03C1 |
HID Keyboard. | |
#define | GAP_APPEARE_HID_MOUSE 0x03C2 |
HID Mouse. | |
#define | GAP_APPEARE_UNKNOWN 0x0000 |
Unknown. | |
#define | GAP_APPEARE_WATCH_SPORTS 0x00C1 |
Watch: Sports Watch. | |
#define | GAP_AUTHENTICATION_COMPLETE_EVENT 0x0A |
#define | GAP_AUTHENTICATION_FAILURE_EVT 0x10 |
#define | GAP_BOND_COMPLETE_EVENT 0x0E |
#define | GAP_CONNECTING_CANCELLED_EVENT 0x15 |
#define | GAP_DEVICE_INIT_DONE_EVENT 0x00 |
#define | GAP_EVT_ADV_DATA_TRUNCATED (uint32_t)BV(6) |
#define | GAP_EVT_ADV_END (uint32_t)BV(3) |
#define | GAP_EVT_ADV_END_AFTER_DISABLE (uint32_t)BV(1) |
#define | GAP_EVT_ADV_EVT_MASK |
Mask for all advertising events. More... | |
#define | GAP_EVT_ADV_REPORT (uint32_t)BV(22) |
#define | GAP_EVT_ADV_REPORT_FULL (uint32_t)BV(23) |
#define | GAP_EVT_ADV_SET_TERMINATED (uint32_t)BV(4) |
#define | GAP_EVT_ADV_START (uint32_t)BV(2) |
#define | GAP_EVT_ADV_START_AFTER_ENABLE (uint32_t)BV(0) |
#define | GAP_EVT_INSUFFICIENT_MEMORY (uint32_t)BV(31) |
A memory failure has occurred. | |
#define | GAP_EVT_SCAN_DISABLED (uint32_t)BV(17) |
#define | GAP_EVT_SCAN_DUR_ENDED (uint32_t)BV(19) |
Scan duration has ended. | |
#define | GAP_EVT_SCAN_ENABLED (uint32_t)BV(16) |
Scanner has been enabled. | |
#define | GAP_EVT_SCAN_EVT_MASK |
Mask for all scan events. More... | |
#define | GAP_EVT_SCAN_INT_ENDED (uint32_t)BV(20) |
#define | GAP_EVT_SCAN_PRD_ENDED (uint32_t)BV(18) |
#define | GAP_EVT_SCAN_REQ_RECEIVED (uint32_t)BV(5) |
#define | GAP_EVT_SCAN_WND_ENDED (uint32_t)BV(21) |
Scan window has ended. | |
#define | GAP_IS_ADDR_RAND(pAddr) |
#define | GAP_IS_ADDR_RPN(pAddr) |
#define | GAP_IS_ADDR_RPR(pAddr) |
#define | GAP_IS_ADDR_RS(pAddr) |
#define | GAP_LINK_ESTABLISHED_EVENT 0x05 |
#define | GAP_LINK_PARAM_UPDATE_EVENT 0x07 |
#define | GAP_LINK_TERMINATED_EVENT 0x06 |
#define | GAP_PAIRING_REQ_EVENT 0x0F |
#define | GAP_PASSKEY_NEEDED_EVENT 0x0B |
#define | GAP_PRIVACY_MODE_DEVICE 1 |
Network Privacy Mode. | |
#define | GAP_PRIVACY_MODE_NETWORK 0 |
Device Privacy Mode. | |
#define | GAP_PROFILE_BROADCASTER 0x01 |
A device that sends advertising events only. | |
#define | GAP_PROFILE_CENTRAL 0x08 |
#define | GAP_PROFILE_OBSERVER 0x02 |
A device that receives advertising events only. | |
#define | GAP_PROFILE_PERIPHERAL 0x04 |
#define | GAP_SCAN_SESSION_END_EVENT 0x12 |
Sent when an advertising report session ends. This is an internal event. | |
#define | GAP_SIGNATURE_UPDATED_EVENT 0x09 |
#define | GAP_SLAVE_REQUESTED_SECURITY_EVENT 0x0C |
#define | GAP_STATE_ADV 0x01 |
Device is advertising. | |
#define | GAP_STATE_IDLE 0x00 |
Device is idle. | |
#define | GAP_STATE_INIT 0x04 |
Device is establishing a connection. | |
#define | GAP_STATE_SCAN 0x02 |
Device is scanning. | |
#define | GAP_UPDATE_LINK_PARAM_REQ_EVENT 0x11 |
#define | MASK_ADDRTYPE_ID 0x01 |
AND with addrtype to remove ID from type. | |
#define | PRIVATE_NON_RESOLVE_ADDR_HDR 0x80 |
Random Private Non-Resolvable Address (b10) | |
#define | PRIVATE_RESOLVE_ADDR_HDR 0x40 |
Random Private Resolvable Address (b01) | |
#define | RANDOM_ADDR_HDR_MASK 0xC0 |
Get top 2 bits of address. | |
#define | SET_ADDRTYPE_ID 0x02 |
OR with addrtype to change addr type to ID. | |
#define | STATIC_ADDR_HDR 0xC0 |
Random Static Address (b11) | |
Typedefs | |
typedef void(* | pfnGapCB_t) (uint32_t event, void *pBuf, uintptr_t arg) |
typedef void(* | pfnGapConnEvtCB_t) (Gap_ConnEventRpt_t *pReport) |
typedef uint8_t(* | pfnGapDevPrivModeCB_t) (GAP_Peer_Addr_Types_t addrType, uint8_t *pAddr) |
GAP Device Privacy Mode Callback Function. | |
typedef void(* | pfnGapIdleCB_t) () |
GAP Idle Callback Function. | |
typedef uint8_t(* | pfnSuppCentAddrRes_t) (uint8_t *deviceAddr, GAP_Peer_Addr_Types_t addrType) |
Central Address Resolution (CAR) Support Callback Function. | |
Functions | |
bStatus_t | GAP_Authenticate (gapAuthParams_t *pParams, gapPairingReq_t *pPairReq) |
bStatus_t | GAP_Bond (uint16_t connectionHandle, uint8_t authenticated, uint8_t secureConnections, smSecurityInfo_t *pParams, uint8_t startEncryption) |
bStatus_t | GAP_DeviceInit (uint8_t profileRole, uint8_t taskID, GAP_Addr_Modes_t addrMode, uint8_t *pRandomAddr) |
uint8_t * | GAP_GetDevAddress (uint8 wantIA) |
uint8_t * | GAP_GetIRK (void) |
uint16_t | GAP_GetParamValue (uint16_t paramID) |
uint8_t * | GAP_GetSRK (void) |
void | GAP_Init (uint8_t task_id) |
uint8_t | GAP_isPairing (void) |
uint8_t | GAP_NumActiveConnections (void) |
bStatus_t | GAP_PasscodeUpdate (uint32_t passcode, uint16_t connectionHandle) |
bStatus_t | GAP_PasskeyUpdate (uint8_t *pPasskey, uint16_t connectionHandle) |
uint16_t | GAP_ProcessEvent (uint8_t task_id, uint16_t events) |
void | GAP_RegisterBondMgrCBs (gapBondMgrCBs_t *pCBs) |
bStatus_t | Gap_RegisterConnEventCb (pfnGapConnEvtCB_t cb, GAP_CB_Action_t action, uint16_t connHandle) |
void | GAP_RegisterForMsgs (uint8_t taskID) |
bStatus_t | GAP_SendSlaveSecurityRequest (uint16_t connectionHandle, uint8_t authReq) |
bStatus_t | GAP_SetParamValue (uint16_t paramID, uint16_t paramValue) |
bStatus_t | GAP_SetPrivacyMode (GAP_Peer_Addr_Types_t addrType, uint8_t *pAddr, uint8_t mode) |
bStatus_t | GAP_Signable (uint16_t connectionHandle, uint8_t authenticated, smSigningInfo_t *pParams) |
bStatus_t | GAP_TerminateAuth (uint16_t connectionHandle, uint8_t reason) |
bStatus_t | GAP_TerminateLinkReq (uint16_t connectionHandle, uint8_t reason) |
bStatus_t | GAP_UpdateLinkParamReq (gapUpdateLinkParamReq_t *pParams) |
bStatus_t | GAP_UpdateLinkParamReqReply (gapUpdateLinkParamReqReply_t *pParams) |
bStatus_t | GapConfig_SetParameter (Gap_configParamIds_t param, void *pValue) |