![]() |
![]() |
TI BLE-Stack for Bluetooth API Documentation
3.03.07.00
|
Macros | |
#define | GAPBOND_PAIRING_STATE_BOND_SAVED 0x03 |
Bonding record saved in NV. | |
#define | GAPBOND_PAIRING_STATE_BONDED 0x02 |
Bonding Complete. More... | |
#define | GAPBOND_PAIRING_STATE_CAR_READ 0x04 |
Central Address Resolution Characteristic Read. | |
#define | GAPBOND_PAIRING_STATE_COMPLETE 0x01 |
Pairing Complete. More... | |
#define | GAPBOND_PAIRING_STATE_STARTED 0x00 |
Pairing Started. More... | |
These are the states that are returned through the pfnPairStateCB_t . See the specific state for its possible statuses.
#define GAPBOND_PAIRING_STATE_BONDED 0x02 |
Bonding Complete.
The following statuses are possible for this state:
#define GAPBOND_PAIRING_STATE_COMPLETE 0x01 |
Pairing Complete.
The following statuses are possible for this state:
#define GAPBOND_PAIRING_STATE_STARTED 0x00 |
Pairing Started.
The following statuses are possible for this state: