![]() |
![]() |
TI BLE-Stack for Bluetooth API Documentation
3.03.07.00
|
Connection Response format. More...
Data Fields | |
uint16 | dstCID |
Represents CID on device receiving request and sending response. | |
uint16 | initCredits |
Indicates number of LE-frames that peer device can send. | |
uint16 | mps |
Specifies maximum payload size that can be received on this channel. | |
uint16 | mtu |
Specifies maximum SDU size that can be received on this channel. | |
uint16 | result |
Indicates outcome of connection request: L2CAP Connection Response Result Values. | |
Connection Response format.