BLE-Stack 3.00.01 to BLE-Stack 3.01.00¶
This section will describe a way to migrate a project from BLE-Stack 3.00.01 to a BLE-Stack 3.01.00 project.
For this migration guide, simple_peripheral from BLE-Stack 3.00.01 will be ported over to BLE-Stack 3.01.00. Because the directory structure is nearly identical between the two releases, the recommended approach is to start with a BLE-Stack 3.01.00 project that contains the same base functionality as the porting target project and merge in any custom functionality.
Choose a BLE-Stack 3.01.00 example project that contains your target project’s base functionality.
For reference, see available sample projects that start with simple_peripheral
In this example, we’re going to use simple_peripheral as the starting BLE-Stack 3.01.00 sample project.
Transfer all modified application files from BLE-Stack 3.00.01 into the BLE-Stack 3.01.00 example project.
In this example, the following files from BLE-Stack 3.00.01 were moved into simple_peripheral BLE-Stack 3.01.00 example:
simple_peripheral.c
simple_peripheral.h
simple_gatt_profile.c
simple_gatt_profile.h
Replace includes of
icall_apimsg.h
andicall_api.h
withicall_ble_api.h
.#include "icall_ble_api.h"
Make sure not to include any of the following files in your project: (They are already included in
icall_ble_api.h
.)gap.h
hci.h
l2cap.h
gatt.h
gattserverapp.h
linkdb.h
att.h
If your code contains any
#ifdef USE_CORE_SDK
, remove these.Modify
main.c
in the BLE-Stack 3.01.00 example if additional tasks were added in the BLE-Stack 3.00.01 project.Please do not add any
DV42_FEATURES
defines tobuild_config.opt
in BLE-Stack 3.01.00. If you want to enable or disable LE Secure Connections, please use theGAPBOND_SECURE_CONNECTION
parameter. (Secure Connections is enabled by default in BLE-Stack 3.01.00.)uint8_t gapbondSecure = GAPBOND_SECURE_CONNECTION_NONE; GAPBondMgr_SetParameter(GAPBOND_SECURE_CONNECTION, sizeof(uint8_t), &gapbondSecure);
In BLE-Stack 3.01.00, heap management has been updated. Please see dynamic_memory_allocation for details on how to optimize your heap.
In BLE-Stack 3.01.00, OAD has been updated. Please see Introduction.
If you are using the GAPBondMgr, make sure a passcode callback function is defined and sent to the GAPBondMgr. This is mandatory in BLE-Stack 3.01.00.
// GAP Bond Manager Callbacks // These are set to NULL since they are not needed. The application // is set up to only perform justworks pairing. static gapBondCBs_t simpleBLEPeripheral_BondMgrCBs = { (pfnPasscodeCB_t) SimpleBLEPeripheral_passcodeCB, // Passcode callback SimpleBLEPeripheral_pairStateCB // Pairing / Bonding state Callback };
The passcode callback and handling can be done the following way:
Define an event
SBP_PASSCODE_NEEDED_EVT
such that theSimpleBLEPeripheral_passcodeCB
function can enqueue a message for the application task to handle.#define SBP_STATE_CHANGE_EVT 0x0001 #define SBP_CHAR_CHANGE_EVT 0x0002 #define SBP_PASSCODE_NEEDED_EVT 0x0003
The callback function will push this event to application task so that the BLE-Stack API call can happen in the application context.
// Forward Declaration static void SimpleBLEPeripheral_passcodeCB(uint8_t *deviceAddr, uint16_t connHandle, uint8_t uiInputs, uint8_t uiOutputs); // Definition /********************************************************************* * @fn SimpleBLEPeripheral_passcodeCB * * @brief Passcode callback. * * @return none */ static void SimpleBLEPeripheral_passcodeCB(uint8_t *deviceAddr, uint16_t connHandle, uint8_t uiInputs, uint8_t uiOutputs) { uint8_t *pData; // Allocate space for the passcode event. if ((pData = ICall_malloc(sizeof(uint8_t)))) { *pData = uiOutputs; // Enqueue the event. SimpleBLEPeripheral_enqueueMsg(SBP_PASSCODE_NEEDED_EVT, 0); } }
Lastly, take the dequeued message in
SimpleBLEPeripheral_processAppMsg
and call the appropriate BLE-Stack API./********************************************************************* * @fn SimpleBLEPeripheral_processAppMsg * * @brief Process an incoming callback from a profile. * * @param pMsg - message to process * * @return None. */ static void SimpleBLEPeripheral_processAppMsg(sbpEvt_t *pMsg) { switch (pMsg->hdr.event) { // . . . case SBP_PASSCODE_NEEDED_EVT: { // Use static passcode uint32_t passcode = 123456; // Send passcode to GAPBondMgr (assuming single connection) GAPBondMgr_PasscodeRsp(0, SUCCESS, passcode); } break; default: // Do nothing. break; } }
If necessary, update the project to use the newer TI-RTOS drivers that are supplied with the SimpleLink CC2640R2 SDK.
The following drivers have changed from BLE-Stack 3.00.01. Please see the changes to these drivers by comparing the supplied headers between those in simplelink_cc2640r2_sdk_1_30_00_25 and those in the SimpleLink CC2640R2 SDK.
ADC
NVS
Display
Attention
The display folder should in BLE-Stack 3.01.00 be included with the path
<ti/display/Display.h>
, not<ti/mw/display/Display.h>
.#include <ti/display/Display.h>
Refer to the Core SDK release notes for additional information and the TI-RTOS examples included with SimpleLink CC2640R2 SDK.
For additional information on how BLE-Stack 3.01.00 uses TI-RTOS see TI-RTOS (RTOS Kernel) Overview
For any utilized TI Drivers, review TI-RTOS Kernel Users Guide and Driver APIs.
Micro BLE Stack¶
The micro BLE Stack API has changed from ub_
to uble_
. For details, see uble.h
.