TI BLE5-Stack API Documentation
1.01.14.00
|
Macros | |
#define | OAD_IMG_HDR_LEN sizeof(imgFixedHdr_t) |
#define | OAD_IMG_ID_LEN 8 |
#define | OAD_SW_VER_LEN 4 |
#define | SEG_HDR_LEN 12 |
#define OAD_IMG_HDR_LEN sizeof(imgFixedHdr_t) |
Length of imgFixedHdr_t, this is the length of the core header
#define OAD_IMG_ID_LEN 8 |
Length of OAD image ID field, this is the length of OAD_IMG_ID_VAL and OAD_EXTFL_ID_VAL
#define OAD_SW_VER_LEN 4 |
Length of software version in bytes
#define SEG_HDR_LEN 12 |
Length of boundarySeg_t in bytes