|
void | AONEventMcuWakeUpSet (uint32_t ui32MCUWUEvent, uint32_t ui32EventSrc) |
| Select event source for the specified MCU wake-up programmable event. More...
|
|
uint32_t | AONEventMcuWakeUpGet (uint32_t ui32MCUWUEvent) |
| Get event source for the specified MCU wake-up programmable event. More...
|
|
void | AONEventAuxWakeUpSet (uint32_t ui32AUXWUEvent, uint32_t ui32EventSrc) |
| Select event source for the specified AUX wake-up programmable event. More...
|
|
uint32_t | AONEventAuxWakeUpGet (uint32_t ui32AUXWUEvent) |
| Get event source for the specified AUX wake-up programmable event. More...
|
|
void | AONEventMcuSet (uint32_t ui32MCUEvent, uint32_t ui32EventSrc) |
| Select event source for the specified programmable event forwarded to the MCU event fabric. More...
|
|
uint32_t | AONEventMcuGet (uint32_t ui32MCUEvent) |
| Get source for the specified programmable event forwarded to the MCU event fabric. More...
|
|
static void | AONEventRtcSet (uint32_t ui32EventSrc) |
| Select event source forwarded to AON Real Time Clock (RTC). More...
|
|
static uint32_t | AONEventRtcGet (void) |
| Get event source forwarded to AON Real Time Clock (RTC). More...
|
|