|
uint32_t | CRYPTOAesLoadKey (uint32_t *pui32AesKey, uint32_t ui32KeyLocation) |
| Write the key into the Key Ram. More...
|
|
uint32_t | CRYPTOAesCbc (uint32_t *pui32MsgIn, uint32_t *pui32MsgOut, uint32_t ui32MsgLength, uint32_t *pui32Nonce, uint32_t ui32KeyLocation, bool bEncrypt, bool bIntEnable) |
| Start an AES-CBC operation (encryption or decryption). More...
|
|
uint32_t | CRYPTOAesCbcStatus (void) |
| Check the result of an AES CBC operation. More...
|
|
uint32_t | CRYPTOAesEcb (uint32_t *pui32MsgIn, uint32_t *pui32MsgOut, uint32_t ui32KeyLocation, bool bEncrypt, bool bIntEnable) |
| Start an AES-ECB operation (encryption or decryption). More...
|
|
uint32_t | CRYPTOAesEcbStatus (void) |
| Check the result of an AES ECB operation. More...
|
|
static void | CRYPTOAesEcbFinish (void) |
| Finish the encryption operation by resetting the operation mode. More...
|
|
static void | CRYPTOAesCbcFinish (void) |
| Finish the encryption operation by resetting the operation mode. More...
|
|
uint32_t | CRYPTOCcmAuthEncrypt (bool bEncrypt, uint32_t ui32AuthLength, uint32_t *pui32Nonce, uint32_t *pui32PlainText, uint32_t ui32PlainTextLength, uint32_t *pui32Header, uint32_t ui32HeaderLength, uint32_t ui32KeyLocation, uint32_t ui32FieldLength, bool bIntEnable) |
| Start CCM operation. More...
|
|
uint32_t | CRYPTOCcmAuthEncryptStatus (void) |
| Check the result of an AES CCM operation. More...
|
|
uint32_t | CRYPTOCcmAuthEncryptResultGet (uint32_t ui32TagLength, uint32_t *pui32CcmTag) |
| Get the result of an AES CCM operation. More...
|
|
uint32_t | CRYPTOCcmInvAuthDecrypt (bool bDecrypt, uint32_t ui32AuthLength, uint32_t *pui32Nonce, uint32_t *pui32CipherText, uint32_t ui32CipherTextLength, uint32_t *pui32Header, uint32_t ui32HeaderLength, uint32_t ui32KeyLocation, uint32_t ui32FieldLength, bool bIntEnable) |
| Start a CCM Decryption and Inverse Authentication operation. More...
|
|
uint32_t | CRYPTOCcmInvAuthDecryptStatus (void) |
| Checks CCM decrypt and Inverse Authentication result. More...
|
|
uint32_t | CRYPTOCcmInvAuthDecryptResultGet (uint32_t ui32AuthLength, uint32_t *pui32CipherText, uint32_t ui32CipherTextLength, uint32_t *pui32CcmTag) |
| Get the result of the CCM operation. More...
|
|
static uint32_t | CRYPTODmaStatus (void) |
| Get the current status of the Crypto DMA controller. More...
|
|
void | CRYPTODmaEnable (uint32_t ui32Channels) |
| Enable Crypto DMA operation. More...
|
|
void | CRYPTODmaDisable (uint32_t ui32Channels) |
| Disable Crypto DMA operation. More...
|
|
static void | CRYPTOIntEnable (uint32_t ui32IntFlags) |
| Enables individual Crypto interrupt sources. More...
|
|
static void | CRYPTOIntDisable (uint32_t ui32IntFlags) |
| Disables individual CRYPTO interrupt sources. More...
|
|
static uint32_t | CRYPTOIntStatus (bool bMasked) |
| Gets the current interrupt status. More...
|
|
static void | CRYPTOIntClear (uint32_t ui32IntFlags) |
| Clears Crypto interrupt sources. More...
|
|
static void | CRYPTOIntRegister (void(*pfnHandler)(void)) |
| Registers an interrupt handler for a Crypto interrupt in the dynamic interrupt table. More...
|
|
static void | CRYPTOIntUnregister (void) |
| Unregisters an interrupt handler for a Crypto interrupt in the dynamic interrupt table. More...
|
|