#include <rf_ble_cmd.h>
Data Fields | |
struct { | |
uint8_t __pad0__:2 | |
uint8_t deviceAddrType:1 | |
The type of the device address – public (0) or random (1) More... | |
} | advConfig |
uint8_t | __dummy0 |
uint8_t | __dummy1 |
uint8_t | auxPtrTargetType |
Number indicating reference for auxPtrTargetTime. Takes same values as trigger types, but only TRIG_ABSTIME and TRIG_REL_* are allowed. More... | |
ratmr_t | auxPtrTargetTime |
Time of start of packet to which auxPtr points. More... | |
uint8_t * | pAdvPkt |
Pointer to extended advertising packet for the ADV_EXT_IND packet. More... | |
uint16_t * | pDeviceAddress |
Pointer (with least significant bit set to 0) to device address used for this device. If least significant bit is 1, the address type given by advConfig.deviceAddrType is inverted. More... | |
uint8_t rfc_ble5AdvExtPar_s::__dummy0 |
uint8_t rfc_ble5AdvExtPar_s::__dummy1 |
uint8_t rfc_ble5AdvExtPar_s::__pad0__ |
struct { ... } rfc_ble5AdvExtPar_s::advConfig |
ratmr_t rfc_ble5AdvExtPar_s::auxPtrTargetTime |
Time of start of packet to which auxPtr points.
uint8_t rfc_ble5AdvExtPar_s::auxPtrTargetType |
Number indicating reference for auxPtrTargetTime. Takes same values as trigger types, but only TRIG_ABSTIME and TRIG_REL_* are allowed.
uint8_t rfc_ble5AdvExtPar_s::deviceAddrType |
The type of the device address – public (0) or random (1)
uint8_t* rfc_ble5AdvExtPar_s::pAdvPkt |
Pointer to extended advertising packet for the ADV_EXT_IND packet.
uint16_t* rfc_ble5AdvExtPar_s::pDeviceAddress |
Pointer (with least significant bit set to 0) to device address used for this device. If least significant bit is 1, the address type given by advConfig.deviceAddrType
is inverted.