#include <rf_ble_cmd.h>
Data Fields | |
uint16_t | nTxScanReq |
Number of transmitted SCAN_REQ packets. More... | |
uint16_t | nBackedOffScanReq |
Number of SCAN_REQ packets not sent due to backoff procedure. More... | |
uint16_t | nRxAdvOk |
Number of ADV*_IND packets received with CRC OK and not ignored. More... | |
uint16_t | nRxAdvIgnored |
Number of ADV*_IND packets received with CRC OK, but ignored. More... | |
uint16_t | nRxAdvNok |
Number of ADV*_IND packets received with CRC error. More... | |
uint16_t | nRxScanRspOk |
Number of SCAN_RSP packets received with CRC OK and not ignored. More... | |
uint16_t | nRxScanRspIgnored |
Number of SCAN_RSP packets received with CRC OK, but ignored. More... | |
uint16_t | nRxScanRspNok |
Number of SCAN_RSP packets received with CRC error. More... | |
uint8_t | nRxAdvBufFull |
Number of ADV*_IND packets received that did not fit in Rx queue. More... | |
uint8_t | nRxScanRspBufFull |
Number of SCAN_RSP packets received that did not fit in Rx queue. More... | |
int8_t | lastRssi |
The RSSI of the last received packet (signed) More... | |
uint8_t | __dummy0 |
ratmr_t | timeStamp |
Time stamp of the last successfully received ADV*_IND packet that was not ignored. More... | |
uint8_t rfc_bleScannerOutput_s::__dummy0 |
int8_t rfc_bleScannerOutput_s::lastRssi |
The RSSI of the last received packet (signed)
uint16_t rfc_bleScannerOutput_s::nBackedOffScanReq |
Number of SCAN_REQ packets not sent due to backoff procedure.
uint8_t rfc_bleScannerOutput_s::nRxAdvBufFull |
Number of ADV*_IND packets received that did not fit in Rx queue.
uint16_t rfc_bleScannerOutput_s::nRxAdvIgnored |
Number of ADV*_IND packets received with CRC OK, but ignored.
uint16_t rfc_bleScannerOutput_s::nRxAdvNok |
Number of ADV*_IND packets received with CRC error.
uint16_t rfc_bleScannerOutput_s::nRxAdvOk |
Number of ADV*_IND packets received with CRC OK and not ignored.
uint8_t rfc_bleScannerOutput_s::nRxScanRspBufFull |
Number of SCAN_RSP packets received that did not fit in Rx queue.
uint16_t rfc_bleScannerOutput_s::nRxScanRspIgnored |
Number of SCAN_RSP packets received with CRC OK, but ignored.
uint16_t rfc_bleScannerOutput_s::nRxScanRspNok |
Number of SCAN_RSP packets received with CRC error.
uint16_t rfc_bleScannerOutput_s::nRxScanRspOk |
Number of SCAN_RSP packets received with CRC OK and not ignored.
uint16_t rfc_bleScannerOutput_s::nTxScanReq |
Number of transmitted SCAN_REQ packets.
ratmr_t rfc_bleScannerOutput_s::timeStamp |
Time stamp of the last successfully received ADV*_IND packet that was not ignored.