|
static void | UARTParityModeSet (uint32_t ui32Base, uint32_t ui32Parity) |
| Sets the type of parity. More...
|
|
static uint32_t | UARTParityModeGet (uint32_t ui32Base) |
| Gets the type of parity currently being used. More...
|
|
static void | UARTFIFOLevelSet (uint32_t ui32Base, uint32_t ui32TxLevel, uint32_t ui32RxLevel) |
| Sets the FIFO level at which interrupts are generated. More...
|
|
void | UARTFIFOLevelGet (uint32_t ui32Base, uint32_t *pui32TxLevel, uint32_t *pui32RxLevel) |
| Gets the FIFO level at which interrupts are generated. More...
|
|
void | UARTConfigSetExpClk (uint32_t ui32Base, uint32_t ui32UARTClk, uint32_t ui32Baud, uint32_t ui32Config) |
| Sets the configuration of a UART. More...
|
|
void | UARTConfigGetExpClk (uint32_t ui32Base, uint32_t ui32UARTClk, uint32_t *pui32Baud, uint32_t *pui32Config) |
| Gets the current configuration of a UART. More...
|
|
static void | UARTEnable (uint32_t ui32Base) |
| Enables transmitting and receiving. More...
|
|
void | UARTDisable (uint32_t ui32Base) |
| Disables transmitting and receiving. More...
|
|
static void | UARTFIFOEnable (uint32_t ui32Base) |
| Enables the transmit and receive FIFOs. More...
|
|
static void | UARTFIFODisable (uint32_t ui32Base) |
| Disables the transmit and receive FIFOs. More...
|
|
static bool | UARTCharsAvail (uint32_t ui32Base) |
| Determines if there are any characters in the receive FIFO. More...
|
|
static bool | UARTSpaceAvail (uint32_t ui32Base) |
| Determines if there is any space in the transmit FIFO. More...
|
|
int32_t | UARTCharGetNonBlocking (uint32_t ui32Base) |
| Receives a character from the specified port. More...
|
|
int32_t | UARTCharGet (uint32_t ui32Base) |
| Waits for a character from the specified port. More...
|
|
bool | UARTCharPutNonBlocking (uint32_t ui32Base, uint8_t ui8Data) |
| Sends a character to the specified port. More...
|
|
void | UARTCharPut (uint32_t ui32Base, uint8_t ui8Data) |
| Waits to send a character from the specified port. More...
|
|
static bool | UARTBusy (uint32_t ui32Base) |
| Determines whether the UART transmitter is busy or not. More...
|
|
static void | UARTBreakCtl (uint32_t ui32Base, bool bBreakState) |
| Causes a BREAK to be sent. More...
|
|
void | UARTIntRegister (uint32_t ui32Base, void(*pfnHandler)(void)) |
| Registers an interrupt handler for a UART interrupt in the dynamic interrupt table. More...
|
|
void | UARTIntUnregister (uint32_t ui32Base) |
| Unregisters an interrupt handler for a UART interrupt in the dynamic interrupt table. More...
|
|
static void | UARTIntEnable (uint32_t ui32Base, uint32_t ui32IntFlags) |
| Enables individual UART interrupt sources. More...
|
|
static void | UARTIntDisable (uint32_t ui32Base, uint32_t ui32IntFlags) |
| Disables individual UART interrupt sources. More...
|
|
static uint32_t | UARTIntStatus (uint32_t ui32Base, bool bMasked) |
| Gets the current interrupt status. More...
|
|
static void | UARTIntClear (uint32_t ui32Base, uint32_t ui32IntFlags) |
| Clears UART interrupt sources. More...
|
|
static void | UARTDMAEnable (uint32_t ui32Base, uint32_t ui32DMAFlags) |
| Enable UART DMA operation. More...
|
|
static void | UARTDMADisable (uint32_t ui32Base, uint32_t ui32DMAFlags) |
| Disable UART DMA operation. More...
|
|
static uint32_t | UARTRxErrorGet (uint32_t ui32Base) |
| Gets current receiver errors. More...
|
|
static void | UARTRxErrorClear (uint32_t ui32Base) |
| Clears all reported receiver errors. More...
|
|
static void | UARTHwFlowControlEnable (uint32_t ui32Base) |
| Enables hardware flow control for both CTS and RTS. More...
|
|
static void | UARTHwFlowControlDisable (uint32_t ui32Base) |
| Disables hardware flow control for both CTS and RTS. More...
|
|