#include <stdbool.h>
#include <stdint.h>
#include "../inc/hw_types.h"
#include "../inc/hw_ints.h"
#include "../inc/hw_memmap.h"
#include "../inc/hw_wdt.h"
#include "debug.h"
#include "interrupt.h"
Macros | |
#define | WATCHDOG_LOCK_UNLOCKED 0x00000000 |
#define | WATCHDOG_LOCK_LOCKED 0x00000001 |
#define | WATCHDOG_LOCK_UNLOCK 0x1ACCE551 |
#define | WATCHDOG_INT_TIMEOUT 0x00000001 |
#define | WATCHDOG_INT_TYPE_INT 0x00000000 |
#define | WATCHDOG_INT_TYPE_NMI 0x00000004 |
Functions | |
static bool | WatchdogRunning (void) |
Determines if the watchdog timer is enabled. More... | |
static void | WatchdogEnable (void) |
Enables the watchdog timer. More... | |
static void | WatchdogResetEnable (void) |
Enables the watchdog timer reset. More... | |
static void | WatchdogResetDisable (void) |
Disables the watchdog timer reset. More... | |
static void | WatchdogLock (void) |
Enables the watchdog timer lock mechanism. More... | |
static void | WatchdogUnlock (void) |
Disables the watchdog timer lock mechanism. More... | |
static bool | WatchdogLockState (void) |
Gets the state of the watchdog timer lock mechanism. More... | |
static void | WatchdogReloadSet (uint32_t ui32LoadVal) |
Sets the watchdog timer reload value. More... | |
static uint32_t | WatchdogReloadGet (void) |
Gets the watchdog timer reload value. More... | |
static uint32_t | WatchdogValueGet (void) |
Gets the current watchdog timer value. More... | |
static void | WatchdogIntRegister (void(*pfnHandler)(void)) |
Registers an interrupt handler for the watchdog timer interrupt in the dynamic interrupt table. More... | |
static void | WatchdogIntUnregister (void) |
Unregisters an interrupt handler for the watchdog timer interrupt in the dynamic interrupt table. More... | |
static void | WatchdogIntEnable (void) |
Enables the watchdog timer. More... | |
static uint32_t | WatchdogIntStatus (void) |
Gets the current watchdog timer interrupt status. More... | |
static void | WatchdogIntClear (void) |
Clears the watchdog timer interrupt. More... | |
static void | WatchdogIntTypeSet (uint32_t ui32Type) |
Sets the type of interrupt generated by the watchdog. More... | |
static void | WatchdogStallEnable (void) |
Enables stalling of the watchdog timer during debug events. More... | |
static void | WatchdogStallDisable (void) |
Disables stalling of the watchdog timer during debug events. More... | |