Data Structures | Macros | Typedefs | Enumerations | Functions | Variables
TRNG.h File Reference

Detailed Description

TRNG driver header.


Warning
This is a beta API. It may change in future releases.

Overview

The True Random Number Generator (TRNG) module generates numbers of variable lengths from a source of entropy. The output is suitable for applications requiring cryptographically random numbers such as keying material for private or symmetric keys.

Usage

Before starting a TRNG operation

Before starting a TRNG operation, the application must do the following:

TRNG operations

TRNG_generateEntropy() provides the most basic functionality. Use it to generate random numbers of a specified width without further restrictions. An example use-case would be generating a symmetric key for AES encryption and / or authentication.

To generate an ECC private key, you should use rejection sampling to ensure that the keying material is in the interval [1, n - 1]. The ECDH public key genreation APIs will reject private keys that are outside of this interval. This information may be used to generate keying material until a suitable key is generated. For most curves, it is improbable to generate a random number outside of this interval because n is a large number close to the maximum number that would fit in the k-byte keying material array. An example of how to do this is given below.

After the TRNG operation completes

After the TRNG operation completes, the application should either start another operation or close the driver by calling TRNG_close().

Synopsis

// Import TRNG Driver definitions
// Define name for TRNG channel index
#define TRNG_INSTANCE 0
#define KEY_LENGTH_BYTES 16
handle = TRNG_open(TRNG_INSTANCE, NULL);
CryptoKeyPlaintext_initBlankKey(&entropyKey, entropyBuffer, KEY_LENGTH_BYTES);
result = TRNG_generateEntropy(handle, &entropyKey);
TRNG_close(handle);

Examples

### Generate symmetric encryption key #

#define KEY_LENGTH_BYTES 16
TRNG_Handle handle;
int_fast16_t result;
CryptoKey entropyKey;
uint8_t entropyBuffer[KEY_LENGTH_BYTES];
handle = TRNG_open(0, NULL);
if (!handle) {
// Handle error
while(1);
}
CryptoKeyPlaintext_initBlankKey(&entropyKey, entropyBuffer, KEY_LENGTH_BYTES);
result = TRNG_generateEntropy(handle, &entropyKey);
if (result != TRNG_STATUS_SUCCESS) {
// Handle error
while(1);
}
TRNG_close(handle);

Generate ECC private and public key using rejection sampling

TRNG_Handle trngHandle;
ECDH_Handle ecdhHandle;
CryptoKey privateKey;
CryptoKey publicKey;
int_fast16_t trngResult;
int_fast16_t ecdhResult;
uint8_t privateKeyingMaterial[32];
uint8_t publicKeyingMaterial[64];
trngHandle = TRNG_open(0, NULL);
if (!trngHandle) {
while(1);
}
ecdhHandle = ECDH_open(0, NULL);
if (!ecdhHandle) {
while(1);
}
// Repeatedly generate random numbers until they are in the range [1, n - 1].
// Since the NIST-P256 order is so close to 2^256, the probability of needing
// to generate more than one random number is incredibly low but not non-zero.
do {
CryptoKeyPlaintext_initBlankKey(&privateKey, privateKeyingMaterial, ECCParams_NISTP256.length);
CryptoKeyPlaintext_initBlankKey(&publicKey, publicKeyingMaterial, 2 * ECCParams_NISTP256.length);
trngResult = TRNG_generateEntropy(trngHandle, &privateKey);
if (trngResult != TRNG_STATUS_SUCCESS) {
while(1);
}
genPubKeyOperation.curve = &ECCParams_NISTP256;
genPubKeyOperation.myPrivateKey = &privateKey;
genPubKeyOperation.myPublicKey = &publicKey;
ecdhResult = ECDH_generatePublicKey(ecdhHandle, &genPubKeyOperation);
TRNG_close(trngHandle);
ECDH_close(ecdhHandle);
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKey.h>
Include dependency graph for TRNG.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  TRNG_Config
 TRNG Global configuration. More...
 
struct  TRNG_Params
 TRNG Parameters. More...
 

Macros

#define TRNG_STATUS_RESERVED   (-32)
 
#define TRNG_STATUS_SUCCESS   (0)
 Successful status code. More...
 
#define TRNG_STATUS_ERROR   (-1)
 Generic error status code. More...
 
#define TRNG_STATUS_RESOURCE_UNAVAILABLE   (-2)
 An error status code returned if the hardware or software resource is currently unavailable. More...
 

Typedefs

typedef struct TRNG_ConfigTRNG_Handle
 A handle that is returned from a TRNG_open() call. More...
 
typedef struct TRNG_Config TRNG_Config
 TRNG Global configuration. More...
 
typedef void(* TRNG_CallbackFxn) (TRNG_Handle handle, int_fast16_t returnValue, CryptoKey *entropy)
 The definition of a callback function used by the TRNG driver when used in TRNG_RETURN_BEHAVIOR_CALLBACK. More...
 

Enumerations

enum  TRNG_ReturnBehavior { TRNG_RETURN_BEHAVIOR_CALLBACK = 1, TRNG_RETURN_BEHAVIOR_BLOCKING = 2, TRNG_RETURN_BEHAVIOR_POLLING = 4 }
 The way in which TRNG function calls return after generating the requested entropy. More...
 

Functions

void TRNG_init (void)
 This function initializes the TRNG module. More...
 
void TRNG_Params_init (TRNG_Params *params)
 Function to initialize the TRNG_Params struct to its defaults. More...
 
TRNG_Handle TRNG_open (uint_least8_t index, TRNG_Params *params)
 This function opens a given TRNG peripheral. More...
 
void TRNG_close (TRNG_Handle handle)
 Function to close a TRNG peripheral specified by the TRNG handle. More...
 
int_fast16_t TRNG_generateEntropy (TRNG_Handle handle, CryptoKey *entropy)
 Generate a random number. More...
 

Variables

const TRNG_Params TRNG_defaultParams
 Default TRNG_Params structure. More...
 

Macro Definition Documentation

§ TRNG_STATUS_RESERVED

#define TRNG_STATUS_RESERVED   (-32)

Common TRNG status code reservation offset. TRNG driver implementations should offset status codes with TRNG_STATUS_RESERVED growing negatively.

Example implementation specific status codes:

#define TRNGXYZ_STATUS_ERROR0 TRNG_STATUS_RESERVED - 0
#define TRNGXYZ_STATUS_ERROR1 TRNG_STATUS_RESERVED - 1
#define TRNGXYZ_STATUS_ERROR2 TRNG_STATUS_RESERVED - 2

§ TRNG_STATUS_SUCCESS

#define TRNG_STATUS_SUCCESS   (0)

Successful status code.

Functions return TRNG_STATUS_SUCCESS if the function was executed successfully.

§ TRNG_STATUS_ERROR

#define TRNG_STATUS_ERROR   (-1)

Generic error status code.

Functions return TRNG_STATUS_ERROR if the function was not executed successfully.

§ TRNG_STATUS_RESOURCE_UNAVAILABLE

#define TRNG_STATUS_RESOURCE_UNAVAILABLE   (-2)

An error status code returned if the hardware or software resource is currently unavailable.

TRNG driver implementations may have hardware or software limitations on how many clients can simultaneously perform operations. This status code is returned if the mutual exclusion mechanism signals that an operation cannot currently be performed.

Typedef Documentation

§ TRNG_Handle

typedef struct TRNG_Config* TRNG_Handle

A handle that is returned from a TRNG_open() call.

§ TRNG_Config

typedef struct TRNG_Config TRNG_Config

TRNG Global configuration.

The TRNG_Config structure contains a set of pointers used to characterize the TRNG driver implementation.

This structure needs to be defined before calling TRNG_init() and it must not be changed thereafter.

See also
TRNG_init()

§ TRNG_CallbackFxn

typedef void(* TRNG_CallbackFxn) (TRNG_Handle handle, int_fast16_t returnValue, CryptoKey *entropy)

The definition of a callback function used by the TRNG driver when used in TRNG_RETURN_BEHAVIOR_CALLBACK.

Parameters
handleHandle of the client that started the TRNG operation.
returnValueReturn status code describing the outcome of the operation.
entropyThe CryptoKey that describes the location the generated entropy will be copied to.

Enumeration Type Documentation

§ TRNG_ReturnBehavior

The way in which TRNG function calls return after generating the requested entropy.

Not all TRNG operations exhibit the specified return behavor. Functions that do not require significant computation and cannot offload that computation to a background thread behave like regular functions. Which functions exhibit the specfied return behavior is not implementation dependent. Specifically, a software-backed implementation run on the same CPU as the application will emulate the return behavior while not actually offloading the computation to the background thread.

TRNG functions exhibiting the specified return behavior have restrictions on the context from which they may be called.

Task Hwi Swi
TRNG_RETURN_BEHAVIOR_CALLBACK X X X
TRNG_RETURN_BEHAVIOR_BLOCKING X
TRNG_RETURN_BEHAVIOR_POLLING X X X
Enumerator
TRNG_RETURN_BEHAVIOR_CALLBACK 

The function call will return immediately while the TRNG operation goes on in the background. The registered callback function is called after the operation completes. The context the callback function is called (task, HWI, SWI) is implementation-dependent.

TRNG_RETURN_BEHAVIOR_BLOCKING 

The function call will block while TRNG operation goes on in the background. TRNG operation results are available after the function returns.

TRNG_RETURN_BEHAVIOR_POLLING 

The function call will continuously poll a flag while TRNG operation goes on in the background. TRNG operation results are available after the function returns.

Function Documentation

§ TRNG_init()

void TRNG_init ( void  )

This function initializes the TRNG module.

Precondition
The TRNG_config structure must exist and be persistent before this function can be called. This function must also be called before any other TRNG driver APIs. This function call does not modify any peripheral registers.

§ TRNG_Params_init()

void TRNG_Params_init ( TRNG_Params params)

Function to initialize the TRNG_Params struct to its defaults.

Parameters
paramsAn pointer to TRNG_Params structure for initialization

Defaults values are: returnBehavior = TRNG_RETURN_BEHAVIOR_BLOCKING callbackFxn = NULL timeout = SemaphoreP_WAIT_FOREVER custom = NULL

§ TRNG_open()

TRNG_Handle TRNG_open ( uint_least8_t  index,
TRNG_Params params 
)

This function opens a given TRNG peripheral.

Precondition
TRNG controller has been initialized using TRNG_init()
Parameters
indexLogical peripheral number for the TRNG indexed into the TRNG_config table
paramsPointer to an parameter block, if NULL it will use default values.
Returns
A TRNG_Handle on success or a NULL on an error or if it has been opened already.
See also
TRNG_init()
TRNG_close()

§ TRNG_close()

void TRNG_close ( TRNG_Handle  handle)

Function to close a TRNG peripheral specified by the TRNG handle.

Precondition
TRNG_open() has to be called first.
Parameters
handleA TRNG handle returned from TRNG_open()
See also
TRNG_open()

§ TRNG_generateEntropy()

int_fast16_t TRNG_generateEntropy ( TRNG_Handle  handle,
CryptoKey entropy 
)

Generate a random number.

Generates a random bitstream of the size defined in the entropy CryptoKey in the range 0 <= entropy buffer < 2 ^ (entropy length * 8). The entropy will be generated and stored according to the storage requirements defined in the CryptoKey.

Precondition
TRNG_open() has to be called first.
Parameters
handleA TRNG handle returned from TRNG_open().
entropyA blank, initialized CryptoKey describing the target location the entropy shall be stored in.
Return values
TRNG_STATUS_SUCCESSThe operation succeeded.
TRNG_STATUS_ERRORThe operation failed.
TRNG_STATUS_RESOURCE_UNAVAILABLEThe required hardware resource was not available. Try again later.

Variable Documentation

§ TRNG_defaultParams

const TRNG_Params TRNG_defaultParams

Default TRNG_Params structure.

See also
TRNG_Params_init()
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale