SimpleLink CC31xx/CC32xx Host Driver
Version 3.0.1.46
Simplifies the implementation of Internet connectivity
|
Data Fields | |
_i16 | LenOrPadding |
_u8 | Sd |
_u8 | FamilyAndFlags |
_u16 | Port |
_u16 | PaddingOrAddr |
_u32 | Address [4] |
Definition at line 839 of file protocol.h.
_u32 Address[4] |
Definition at line 846 of file protocol.h.
_u8 FamilyAndFlags |
Definition at line 843 of file protocol.h.
_i16 LenOrPadding |
Definition at line 841 of file protocol.h.
_u16 PaddingOrAddr |
Definition at line 845 of file protocol.h.
_u16 Port |
Definition at line 844 of file protocol.h.
_u8 Sd |
Definition at line 842 of file protocol.h.