CaptureCC32XX_Object.
More...
#include <CaptureCC32XX.h>
CaptureCC32XX_Object.
The application must not access any member variables of this structure!
§ hwiHandle
HwiP_Handle CaptureCC32XX_Object::hwiHandle |
§ notifyObj
§ callBack
§ periodUnits
§ mode
uint32_t CaptureCC32XX_Object::mode |
§ timer
uint32_t CaptureCC32XX_Object::timer |
§ previousCount
uint32_t CaptureCC32XX_Object::previousCount |
§ isRunning
bool CaptureCC32XX_Object::isRunning |
The documentation for this struct was generated from the following file: