Data Fields
CryptoCC32XX_Config Struct Reference

Crypto Global configuration. More...

#include <CryptoCC32XX.h>

Data Fields

void * object
 

Detailed Description

Crypto Global configuration.

The CryptoCC32XX_Config structure contains a set of pointers used to characterize the Crypto driver implementation.

This structure needs to be defined before calling CryptoCC32XX_init() and it must not be changed thereafter.

See also
CryptoCC32XX_init()

Field Documentation

§ object

void* CryptoCC32XX_Config::object

Pointer to a driver specific data object


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale