Data Fields
CryptoCC32XX_Object Struct Reference

CryptoCC32XX Object. More...

#include <CryptoCC32XX.h>

Data Fields

HwiP_Handle hwiHandle [3]
 
bool isOpen
 
SemaphoreP_Handle sem [3]
 

Detailed Description

CryptoCC32XX Object.

The application must not access any member variables of this structure!

Field Documentation

§ hwiHandle

HwiP_Handle CryptoCC32XX_Object::hwiHandle[3]

Interrupt handles

§ isOpen

bool CryptoCC32XX_Object::isOpen

flag to indicate module is open

§ sem

SemaphoreP_Handle CryptoCC32XX_Object::sem[3]

Semaphore handles


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale