Data Fields
PWM_Params Struct Reference

PWM Parameters. More...

#include <PWM.h>

Data Fields

PWM_Period_Units periodUnits
 
uint32_t periodValue
 
PWM_Duty_Units dutyUnits
 
uint32_t dutyValue
 
PWM_IdleLevel idleLevel
 
void * custom
 

Detailed Description

PWM Parameters.

PWM Parameters are used to with the PWM_open() call. Default values for these parameters are set using PWM_Params_init().

See also
PWM_Params_init()

Field Documentation

§ periodUnits

PWM_Period_Units PWM_Params::periodUnits

Units in which the period is specified

§ periodValue

uint32_t PWM_Params::periodValue

PWM initial period

§ dutyUnits

PWM_Duty_Units PWM_Params::dutyUnits

Units in which the duty is specified

§ dutyValue

uint32_t PWM_Params::dutyValue

PWM initial duty

§ idleLevel

PWM_IdleLevel PWM_Params::idleLevel

Pin output when PWM is stopped.

§ custom

void* PWM_Params::custom

Custom argument used by driver implementation


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale