Data Fields
PowerCC32XX_ParkInfo Struct Reference

Used to specify parking of a pin during LPDS. More...

#include <PowerCC32XX.h>

Data Fields

uint32_t pin
 
uint32_t parkState
 

Detailed Description

Used to specify parking of a pin during LPDS.

Field Documentation

§ pin

uint32_t PowerCC32XX_ParkInfo::pin

The pin to be parked

§ parkState

uint32_t PowerCC32XX_ParkInfo::parkState

The state to park the pin (an enumerated PowerCC32XX_ParkState)


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale