Data Fields
SD_Params Struct Reference

SD Parameters. More...

#include <SD.h>

Data Fields

void * custom
 

Detailed Description

SD Parameters.

SD Parameters are used to with the SD_open() call. Default values for these parameters are set using SD_Params_init().

See also
SD_Params_init()

Field Documentation

§ custom

void* SD_Params::custom

Custom argument used by driver implementation


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale