Data Fields
UART2_Config_ Struct Reference

UART2 Global configuration. More...

#include <UART2.h>

Data Fields

void * object
 
void const * hwAttrs
 

Detailed Description

UART2 Global configuration.

The UART2_Config structure contains a set of pointers used to characterize the UART2 driver implementation.

Field Documentation

§ object

void* UART2_Config_::object

Pointer to a driver specific data object

§ hwAttrs

void const* UART2_Config_::hwAttrs

Pointer to a driver specific hardware attributes structure


The documentation for this struct was generated from the following file:
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale