SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
_SlNetAppHttpServerPostToken_t Struct Reference

Data Fields

_u8 PostActionLen
 
_u8 TokenNameLen
 
_u8 TokenValueLen
 
_u8 padding
 

Detailed Description

Definition at line 979 of file protocol.h.

Field Documentation

§ padding

_u8 padding

Definition at line 984 of file protocol.h.

§ PostActionLen

_u8 PostActionLen

Definition at line 981 of file protocol.h.

§ TokenNameLen

_u8 TokenNameLen

Definition at line 982 of file protocol.h.

§ TokenValueLen

_u8 TokenValueLen

Definition at line 983 of file protocol.h.


The documentation for this struct was generated from the following file: