SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
_SlSpawnMsgItem_s Struct Reference

Data Fields

_SlSpawnEntryFunc_t AsyncHndlr
 
_u8 ActionIndex
 
void * Buffer
 
struct _SlSpawnMsgItem_snext
 

Detailed Description

Definition at line 186 of file driver.h.

Field Documentation

§ ActionIndex

_u8 ActionIndex

Definition at line 189 of file driver.h.

§ AsyncHndlr

_SlSpawnEntryFunc_t AsyncHndlr

Definition at line 188 of file driver.h.

§ Buffer

void* Buffer

Definition at line 190 of file driver.h.

§ next

struct _SlSpawnMsgItem_s* next

Definition at line 191 of file driver.h.


The documentation for this struct was generated from the following file: