SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
_SlSyncPattern_t Struct Reference

Data Fields

_u32 Long
 
_u16 Short
 
_u8 Byte1
 
_u8 Byte2
 

Detailed Description

Definition at line 89 of file protocol.h.

Field Documentation

§ Byte1

_u8 Byte1

Definition at line 93 of file protocol.h.

§ Byte2

_u8 Byte2

Definition at line 94 of file protocol.h.

§ Long

_u32 Long

Definition at line 91 of file protocol.h.

§ Short

_u16 Short

Definition at line 92 of file protocol.h.


The documentation for this struct was generated from the following file: