SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
_StellarisSsiSizeSet_t Struct Reference

Data Fields

_u8 SsiSizeInBytes
 
_u8 Padding [3]
 

Detailed Description

Definition at line 521 of file protocol.h.

Field Documentation

§ Padding

_u8 Padding[3]

Definition at line 524 of file protocol.h.

§ SsiSizeInBytes

_u8 SsiSizeInBytes

Definition at line 523 of file protocol.h.


The documentation for this struct was generated from the following file: