SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
SlFsBundleControlCommand_t Struct Reference

Data Fields

_u16 IncludeFileFilters
 
_u8 Operation
 
_u8 Padding
 

Detailed Description

Definition at line 1243 of file protocol.h.

Field Documentation

§ IncludeFileFilters

_u16 IncludeFileFilters

Definition at line 1245 of file protocol.h.

§ Operation

_u8 Operation

Definition at line 1246 of file protocol.h.

§ Padding

_u8 Padding

Definition at line 1247 of file protocol.h.


The documentation for this struct was generated from the following file: