SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
SlGetSockOptResponse_t Struct Reference

Data Fields

_i16 Status
 
_u8 Sd
 
_u8 OptionLen
 

Detailed Description

Definition at line 922 of file protocol.h.

Field Documentation

§ OptionLen

_u8 OptionLen

Definition at line 926 of file protocol.h.

§ Sd

_u8 Sd

Definition at line 925 of file protocol.h.

§ Status

_i16 Status

Definition at line 924 of file protocol.h.


The documentation for this struct was generated from the following file: