SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
SlNetUtilCmd_t Struct Reference

Data Fields

_u16 Cmd
 
_u16 AttribLen
 
_u16 InputLen
 
_u16 OutputLen
 

Detailed Description

Definition at line 1320 of file protocol.h.

Field Documentation

§ AttribLen

_u16 AttribLen

Definition at line 1323 of file protocol.h.

§ Cmd

_u16 Cmd

Definition at line 1322 of file protocol.h.

§ InputLen

_u16 InputLen

Definition at line 1324 of file protocol.h.

§ OutputLen

_u16 OutputLen

Definition at line 1325 of file protocol.h.


The documentation for this struct was generated from the following file: