SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
SlNetUtilCmdRsp_t Struct Reference

Data Fields

_u32 ObjId
 
_i16 Status
 
_u16 Cmd
 
_u16 OutputLen
 
_u8 Padding [2]
 

Detailed Description

Definition at line 1329 of file protocol.h.

Field Documentation

§ Cmd

_u16 Cmd

Definition at line 1333 of file protocol.h.

§ ObjId

_u32 ObjId

Definition at line 1331 of file protocol.h.

§ OutputLen

_u16 OutputLen

Definition at line 1334 of file protocol.h.

§ Padding

_u8 Padding[2]

Definition at line 1335 of file protocol.h.

§ Status

_i16 Status

Definition at line 1332 of file protocol.h.


The documentation for this struct was generated from the following file: