SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
SlNetUtilSetGet_t Struct Reference

Data Fields

_u32 ObjId
 
_i16 Status
 
_u16 Option
 
_u16 ValueLen
 
_u8 Padding [2]
 

Detailed Description

Definition at line 1309 of file protocol.h.

Field Documentation

§ ObjId

_u32 ObjId

Definition at line 1311 of file protocol.h.

§ Option

_u16 Option

Definition at line 1313 of file protocol.h.

§ Padding

_u8 Padding[2]

Definition at line 1315 of file protocol.h.

§ Status

_i16 Status

Definition at line 1312 of file protocol.h.

§ ValueLen

_u16 ValueLen

Definition at line 1314 of file protocol.h.


The documentation for this struct was generated from the following file: