SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
SlSetSockOptCommand_t Struct Reference

Data Fields

_u8 Sd
 
_u8 Level
 
_u8 OptionName
 
_u8 OptionLen
 

Detailed Description

Definition at line 906 of file protocol.h.

Field Documentation

§ Level

_u8 Level

Definition at line 909 of file protocol.h.

§ OptionLen

_u8 OptionLen

Definition at line 911 of file protocol.h.

§ OptionName

_u8 OptionName

Definition at line 910 of file protocol.h.

§ Sd

_u8 Sd

Definition at line 908 of file protocol.h.


The documentation for this struct was generated from the following file: