SimpleLink CC31xx/CC32xx Host Driver
Version 3.0.1.71
Simplifies the implementation of Internet connectivity
|
Data Fields | |
_i16 | LenOrPadding |
_u8 | Sd |
_u8 | FamilyAndFlags |
_u16 | Port |
_u8 | Address [6] |
Definition at line 834 of file protocol.h.
_u8 Address[6] |
Definition at line 840 of file protocol.h.
_u8 FamilyAndFlags |
Definition at line 838 of file protocol.h.
_i16 LenOrPadding |
Definition at line 836 of file protocol.h.
_u16 Port |
Definition at line 839 of file protocol.h.
_u8 Sd |
Definition at line 837 of file protocol.h.