SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.71
Simplifies the implementation of Internet connectivity
SlSocketCommand_t Struct Reference

Data Fields

_u8 Domain
 
_u8 Type
 
_u8 Protocol
 
_u8 Padding
 

Detailed Description

Definition at line 772 of file protocol.h.

Field Documentation

§ Domain

_u8 Domain

Definition at line 774 of file protocol.h.

§ Padding

_u8 Padding

Definition at line 777 of file protocol.h.

§ Protocol

_u8 Protocol

Definition at line 776 of file protocol.h.

§ Type

_u8 Type

Definition at line 775 of file protocol.h.


The documentation for this struct was generated from the following file: