![]() |
![]() |
UARTCC32XXDMA Hardware attributes. More...
#include <UARTCC32XXDMA.h>
Data Fields | |
unsigned int | baseAddr |
unsigned int | intNum |
unsigned int | intPriority |
uint32_t | flowControl |
unsigned long | rxChannelIndex |
unsigned long | txChannelIndex |
uint16_t | rxPin |
uint16_t | txPin |
uint16_t | ctsPin |
uint16_t | rtsPin |
UARTCC32XXDMA_ErrorCallback | errorFxn |
UARTCC32XXDMA Hardware attributes.
These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For CC32XXWare these definitions are found in:
intPriority is the UART peripheral's interrupt priority, as defined by the underlying OS. It is passed unmodified to the underlying OS's interrupt handler creation code, so you need to refer to the OS documentation for usage. For example, for SYS/BIOS applications, refer to the ti.sysbios.family.arm.m3.Hwi documentation for SYS/BIOS usage of interrupt priorities. If the driver uses the ti.dpl interface instead of making OS calls directly, then the HwiP port handles the interrupt priority in an OS specific way. In the case of the SYS/BIOS port, intPriority is passed unmodified to Hwi_create().
A sample structure is shown below:
unsigned int UARTCC32XXDMA_HWAttrsV1::baseAddr |
UART Peripheral's base address
unsigned int UARTCC32XXDMA_HWAttrsV1::intNum |
UART Peripheral's interrupt vector
unsigned int UARTCC32XXDMA_HWAttrsV1::intPriority |
UART Peripheral's interrupt priority
uint32_t UARTCC32XXDMA_HWAttrsV1::flowControl |
Hardware flow control setting defined by driverlib
unsigned long UARTCC32XXDMA_HWAttrsV1::rxChannelIndex |
uDMA controlTable receive channel index
unsigned long UARTCC32XXDMA_HWAttrsV1::txChannelIndex |
uDMA controlTable transmit channel index
uint16_t UARTCC32XXDMA_HWAttrsV1::rxPin |
UART RX pin assignment
uint16_t UARTCC32XXDMA_HWAttrsV1::txPin |
UART TX pin assignment
uint16_t UARTCC32XXDMA_HWAttrsV1::ctsPin |
UART clear to send (CTS) pin assignment
uint16_t UARTCC32XXDMA_HWAttrsV1::rtsPin |
UART request to send (RTS) pin assignment
UARTCC32XXDMA_ErrorCallback UARTCC32XXDMA_HWAttrsV1::errorFxn |
Application error function to be called on receive errors. Note: The UARTCC32XXDMA driver currently does not use this function.