Data Fields
UARTCC32XXDMA_Object Struct Reference

UARTCC32XXDMA Object. More...

#include <UARTCC32XXDMA.h>

Collaboration diagram for UARTCC32XXDMA_Object:
Collaboration graph
[legend]

Data Fields

bool opened
 
UART_Mode readMode
 
UART_Mode writeMode
 
unsigned int readTimeout
 
unsigned int writeTimeout
 
UART_Callback readCallback
 
UART_Callback writeCallback
 
UART_ReturnMode readReturnMode
 
UART_DataMode readDataMode
 
UART_DataMode writeDataMode
 
uint32_t baudRate
 
UART_LEN dataLength
 
UART_STOP stopBits
 
UART_PAR parityType
 
UART_Echo readEcho
 
const void * writeBuf
 
size_t writeCount
 
size_t writeSize
 
void * readBuf
 
size_t readCount
 
size_t readSize
 
SemaphoreP_Handle writeSem
 
SemaphoreP_Handle readSem
 
HwiP_Handle hwiHandle
 
ClockP_Handle txFifoEmptyClk
 
Power_NotifyObj postNotify
 
unsigned int powerMgrId
 
PowerCC32XX_ParkState prevParkTX
 
uint16_t txPin
 
PowerCC32XX_ParkState prevParkRTS
 
uint16_t rtsPin
 
UDMACC32XX_Handle dmaHandle
 

Detailed Description

UARTCC32XXDMA Object.

The application must not access any member variables of this structure!

Field Documentation

§ opened

bool UARTCC32XXDMA_Object::opened

§ readMode

UART_Mode UARTCC32XXDMA_Object::readMode

§ writeMode

UART_Mode UARTCC32XXDMA_Object::writeMode

§ readTimeout

unsigned int UARTCC32XXDMA_Object::readTimeout

§ writeTimeout

unsigned int UARTCC32XXDMA_Object::writeTimeout

§ readCallback

UART_Callback UARTCC32XXDMA_Object::readCallback

§ writeCallback

UART_Callback UARTCC32XXDMA_Object::writeCallback

§ readReturnMode

UART_ReturnMode UARTCC32XXDMA_Object::readReturnMode

§ readDataMode

UART_DataMode UARTCC32XXDMA_Object::readDataMode

§ writeDataMode

UART_DataMode UARTCC32XXDMA_Object::writeDataMode

§ baudRate

uint32_t UARTCC32XXDMA_Object::baudRate

§ dataLength

UART_LEN UARTCC32XXDMA_Object::dataLength

§ stopBits

UART_STOP UARTCC32XXDMA_Object::stopBits

§ parityType

UART_PAR UARTCC32XXDMA_Object::parityType

§ readEcho

UART_Echo UARTCC32XXDMA_Object::readEcho

§ writeBuf

const void* UARTCC32XXDMA_Object::writeBuf

§ writeCount

size_t UARTCC32XXDMA_Object::writeCount

§ writeSize

size_t UARTCC32XXDMA_Object::writeSize

§ readBuf

void* UARTCC32XXDMA_Object::readBuf

§ readCount

size_t UARTCC32XXDMA_Object::readCount

§ readSize

size_t UARTCC32XXDMA_Object::readSize

§ writeSem

SemaphoreP_Handle UARTCC32XXDMA_Object::writeSem

§ readSem

SemaphoreP_Handle UARTCC32XXDMA_Object::readSem

§ hwiHandle

HwiP_Handle UARTCC32XXDMA_Object::hwiHandle

§ txFifoEmptyClk

ClockP_Handle UARTCC32XXDMA_Object::txFifoEmptyClk

§ postNotify

Power_NotifyObj UARTCC32XXDMA_Object::postNotify

§ powerMgrId

unsigned int UARTCC32XXDMA_Object::powerMgrId

§ prevParkTX

PowerCC32XX_ParkState UARTCC32XXDMA_Object::prevParkTX

§ txPin

uint16_t UARTCC32XXDMA_Object::txPin

§ prevParkRTS

PowerCC32XX_ParkState UARTCC32XXDMA_Object::prevParkRTS

§ rtsPin

uint16_t UARTCC32XXDMA_Object::rtsPin

§ dmaHandle

UDMACC32XX_Handle UARTCC32XXDMA_Object::dmaHandle

The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale