![]() |
![]() |
|
Network Services API
2.80.00.17
|
Managing and monitoring network connections. More...
Data Structures | |
| struct | SlNetConn_config_t |
| Global parameters and attributes used to establish connections. More... | |
Typedefs | |
| typedef void(* | SlNetConn_AppEvent_f) (uint32_t ifID, SlNetConnStatus_e netStatus, void *data) |
| typedef struct SlNetConn_config_t | SlNetConn_config_t |
| Global parameters and attributes used to establish connections. More... | |
Enumerations | |
| enum | SlNetConnServiceLevel_e { SLNETCONN_SERVICE_LVL_MAC = 0, SLNETCONN_SERVICE_LVL_IP = 1, SLNETCONN_SERVICE_LVL_INTERNET = 2 } |
| enum | SlNetConnStatus_e { SLNETCONN_STATUS_DISCONNECTED = 1, SLNETCONN_STATUS_WAITING_FOR_CONNECTION = 2, SLNETCONN_STATUS_CONNECTED = 3, SLNETCONN_STATUS_CONNECTED_MAC = SLNETCONN_STATUS_CONNECTED + SLNETCONN_SERVICE_LVL_MAC, SLNETCONN_STATUS_CONNECTED_IP = SLNETCONN_STATUS_CONNECTED + SLNETCONN_SERVICE_LVL_IP, SLNETCONN_STATUS_CONNECTED_INTERNET = SLNETCONN_STATUS_CONNECTED + SLNETCONN_SERVICE_LVL_INTERNET } |
Functions | |
| int32_t | SlNetConn_init (int32_t flags) |
| Initialize the SlNetConn module. More... | |
| int32_t | SlNetConn_setConfiguration (SlNetConn_config_t *pConf) |
| Sets the SlNetConn global configuration parameters. More... | |
| int32_t | SlNetConn_start (SlNetConnServiceLevel_e targetServiceLevel, SlNetConn_AppEvent_f fAppEventHdl, uint32_t timeout, uint32_t flags) |
| Request a connection (of specific target level) to be establish. More... | |
| int32_t | SlNetConn_stop (SlNetConn_AppEvent_f fAppEventHdl) |
| Remove user's connection request. More... | |
| int32_t | SlNetConn_waitForConnection (SlNetConnServiceLevel_e targetServiceLevel, uint32_t timeout) |
| Wait for connection (of specific target level) to be establish. More... | |
| int32_t | SlNetConn_getStatus (bool bCheckInternetConnection, SlNetConnStatus_e *pStatus) |
| Retrieve the current connection status. More... | |
| void * | SlNetConn_process (void *pvParameters) |
| SlNetConn_process callback - Connection manager thread, handles all connection requests. More... | |
Managing and monitoring network connections.
| typedef void(* SlNetConn_AppEvent_f) (uint32_t ifID, SlNetConnStatus_e netStatus, void *data) |
Application callback function prototype.
This function is per application and is called by the connection manager when an event occurs after the connection is established.
| typedef struct SlNetConn_config_t SlNetConn_config_t |
Global parameters and attributes used to establish connections.
This structure is set using the SlNetConn_setConfiguration(). If the function is not called the default values will apply.
| enum SlNetConnStatus_e |
| int32_t SlNetConn_init | ( | int32_t | flags | ) |
Initialize the SlNetConn module.
SlNetConn_init() initializes the SlNetConn module. Internally, this includes:
This function is called by the application layer and can be called only once
| [in] | flags | Reserved |
| int32_t SlNetConn_setConfiguration | ( | SlNetConn_config_t * | pConf | ) |
Sets the SlNetConn global configuration parameters.
The use of this function is optional. If not called, SlNetConn will use the default configuration.
SlNetConn_setConfiguration() can only be called after SlNetConn_init() and before SlNetConn_start().
| [in] | pConf | SlNetConn configuration (see SlNetConn_config_t) |
| int32_t SlNetConn_start | ( | SlNetConnServiceLevel_e | targetServiceLevel, |
| SlNetConn_AppEvent_f | fAppEventHdl, | ||
| uint32_t | timeout, | ||
| uint32_t | flags | ||
| ) |
Request a connection (of specific target level) to be establish.
SlNetConn_start() passes the connection manager a request to start a connection.
The connection request is valid until SlNetConn_stop() is called.
The fAppEventHdl identifies the request (same "fAppEventHdl" should be used in the SlNetConn_stop()).
The function is blocking (with timeout) until the requested connection is established or until the timeout expires (if timeout is 0, the function will return immediately). Timeout expiration doesn't cancel the request. The Start Connection handles temporary disconnections ("link down"). The user will get a "Disconnection" indication through the fAppEventHdl, but the connection is expected to re-established automatically (when possible). Following the return of the function, the user will be notified through the event handler on the "Connection" and "Disconnection" events. Upon disconnection, the user may use SlNetConn_waitForConnection() to block the execution until the link is up again.
This function can be called from several threads.
This function must be called after SlNetConn_init() and SlNetConn_setConfiguration().
| [in] | targetServiceLevel | Specifies the requested connection level |
| [in] | fAppEventHdl | Pointer to user callback function. A unique callback should be used per SlNetConn_start() request. The callback identifies the user request and should be used upon SlNetConn_stop(). |
| [in] | timeout | Is an upper bound (in seconds) for the time the SlNetConn_start() can be blocked. 0 means non-blocking command - The command will return immediately. Value above 0xffff seconds mean infinity timeout. |
| [in] | flags | reserved |
| int32_t SlNetConn_stop | ( | SlNetConn_AppEvent_f | fAppEventHdl | ) |
Remove user's connection request.
SlNetConn_stop() cancels a connection request (identified by user event handler). When the last user request is being removed, a disconnection will be triggered. This function is non-blocking and called by the application layer. This function must be called after SlNetConn_init() and SlNetConn_setConfiguration().
| [in] | fAppEventHdl | Pointer to user callback function. This should be a unique Callback pointer that corresponds to specific SlNetConn_start() request. |
| int32_t SlNetConn_waitForConnection | ( | SlNetConnServiceLevel_e | targetServiceLevel, |
| uint32_t | timeout | ||
| ) |
Wait for connection (of specific target level) to be establish.
SlNetConn_waitForConnection() waits until the requested connection is established. The function doesn't change user requests status and doesn't trigger a connection. It must follow a SlNetConn_start() with similar (or higher) target service level. This function is blocking. This function can be called from several threads. This function must be called after SlNetConn_init() and SlNetConn_setConfiguration().
| [in] | targetServiceLevel | Specifies the requested connection level |
| [in] | timeout | Is an upper bound (in seconds) for the time the SlNetConn_waitForConnection() can be blocked. 0 means non-blocking command. The command will return immediately. The return code can still be '1' (i.e. Timeout), if the connection setup is in progress. Value above 0xffff seconds mean infinity timeout. |
| int32_t SlNetConn_getStatus | ( | bool | bCheckInternetConnection, |
| SlNetConnStatus_e * | pStatus | ||
| ) |
Retrieve the current connection status.
This will be used by the user poll the current status of the connection manager. If an IP level of connection is already established, the bCheckInternetConnection can be set to request the SlNetConn to check whether an internet access is available.
| [in] | bCheckInternetConnection | Perform internet connection (if IP Address is Acquired) before reporting the active service level. |
| [out] | pStatus | The current active service level |
| void* SlNetConn_process | ( | void * | pvParameters | ) |
SlNetConn_process callback - Connection manager thread, handles all connection requests.
This is the main thread context of the SlNetConn, it will be used to process SlNetIf events and to invoke application's callbacks.
| [in] | pvParameters | Task parameters (should be kept null). |
The thread (that uses this function) needs to be created by the application before SlNetConn_start() is called.