![]() |
![]() |
AESCommonLPF3 Object. More...
#include <AESCommonLPF3.h>
Data Fields | |
uint32_t | semaphoreTimeout |
CryptoKey | key |
volatile int_fast16_t | returnStatus |
AES_ReturnBehavior | returnBehavior |
bool | isOpen |
volatile bool | cryptoResourceLocked |
volatile bool | operationInProgress |
volatile bool | powerConstraintSet |
AESCommonLPF3 Object.
The application must not access any member variables of this structure!
uint32_t AESCommonLPF3_Object::semaphoreTimeout |
CryptoKey AESCommonLPF3_Object::key |
volatile int_fast16_t AESCommonLPF3_Object::returnStatus |
AES_ReturnBehavior AESCommonLPF3_Object::returnBehavior |
bool AESCommonLPF3_Object::isOpen |
volatile bool AESCommonLPF3_Object::cryptoResourceLocked |
volatile bool AESCommonLPF3_Object::operationInProgress |
volatile bool AESCommonLPF3_Object::powerConstraintSet |