TI BLE5-Stack API Documentation
3.02.04.00
|
LE Periodic Advertising Report event. More...
Data Fields | |
uint8 | BLEEventCode |
BLE Event Code. | |
uint8 | cteType |
CTE type received. | |
uint8 * | data |
Periodic data received from peer. | |
uint8 | dataLen |
Periodic data length. | |
uint8 | dataStatus |
Periodic data status. | |
osal_event_hdr_t | hdr |
osal event header | |
int8 | rssi |
RSSI of the received packet. | |
uint16 | syncHandle |
sync handle | |
int8 | txPower |
Tx Power information. | |
LE Periodic Advertising Report event.