![]() |
![]() |
|
TI BLE5-Stack API Documentation
3.03.01.00
|
Macros | |
| #define | ATT_ERROR_RSP 0x01 |
| ATT Error Response. This method is passed as a gattMsgEvent_t defined as attErrorRsp_t. | |
| #define | ATT_EXCHANGE_MTU_REQ 0x02 |
| ATT Exchange MTU Request. This method is passed as a GATT message defined as attExchangeMTUReq_t. | |
| #define | ATT_EXCHANGE_MTU_RSP 0x03 |
| ATT Exchange MTU Response. This method is passed as a GATT message defined as attExchangeMTURsp_t. | |
| #define | ATT_EXECUTE_WRITE_REQ 0x18 |
| ATT Execute Write Request. This method is passed as a GATT message defined as attExecuteWriteReq_t. | |
| #define | ATT_EXECUTE_WRITE_RSP 0x19 |
| ATT Execute Write Response. This method is passed as a GATT message defines as attErrorRsp_t. | |
| #define | ATT_FIND_BY_TYPE_VALUE_REQ 0x06 |
| ATT Find By Type Value Request. This method is passed as a GATT message defined as attFindByTypeValueReq_t. | |
| #define | ATT_FIND_BY_TYPE_VALUE_RSP 0x07 |
| ATT Find By Type Value Response. This method is passed as a GATT message defined as attFindByTypeValueRsp_t. | |
| #define | ATT_FIND_INFO_REQ 0x04 |
| ATT Find Information Request. This method is passed as a GATT message defined as attFindInfoReq_t. | |
| #define | ATT_FIND_INFO_RSP 0x05 |
| ATT Find Information Response. This method is passed as a GATT message defined as attFindInfoRsp_t. | |
| #define | ATT_HANDLE_VALUE_CFM 0x1e |
| ATT Handle Value Confirmation. This method is passed as a GATT message. | |
| #define | ATT_HANDLE_VALUE_IND 0x1d |
| ATT Handle Value Indication. This method is passed as a GATT message defined as attHandleValueInd_t. | |
| #define | ATT_HANDLE_VALUE_NOTI 0x1b |
| ATT Handle Value Notification. This method is passed as a GATT message defined as attHandleValueNoti_t. | |
| #define | ATT_PREPARE_WRITE_REQ 0x16 |
| ATT Prepare Write Request. This method is passed as a GATT message defined as attPrepareWriteReq_t. | |
| #define | ATT_PREPARE_WRITE_RSP 0x17 |
| ATT Prepare Write Response. This method is passed as a GATT message defined as attPrepareWriteRsp_t. | |
| #define | ATT_READ_BLOB_REQ 0x0c |
| ATT Read Blob Request. This method is passed as a GATT message defined as attReadBlobReq_t. | |
| #define | ATT_READ_BLOB_RSP 0x0d |
| ATT Read Blob Response. This method is passed as a GATT message defined as attReadBlobRsp_t. | |
| #define | ATT_READ_BY_GRP_TYPE_REQ 0x10 |
| ATT Read By Group Type Request. This method is passed as a GATT message defined as attReadByGrpTypeReq_t. | |
| #define | ATT_READ_BY_GRP_TYPE_RSP 0x11 |
| ATT Read By Group Type Response. This method is passed as a GATT message defined as attReadByGrpTypeRsp_t. | |
| #define | ATT_READ_BY_TYPE_REQ 0x08 |
| ATT Read By Type Request. This method is passed as a GATT message defined as attReadByTypeReq_t. | |
| #define | ATT_READ_BY_TYPE_RSP 0x09 |
| ATT Read By Type Response. This method is passed as a GATT message defined as attReadByTypeRsp_t. | |
| #define | ATT_READ_MULTI_REQ 0x0e |
| ATT Read Multiple Request. This method is passed as a GATT message defined as attReadMultiReq_t. | |
| #define | ATT_READ_MULTI_RSP 0x0f |
| ATT Read Multiple Response. This method is passed as a GATT message defined as attReadMultiRsp_t. | |
| #define | ATT_READ_REQ 0x0a |
| ATT Read Request. This method is passed as a GATT message defined as attReadReq_t. | |
| #define | ATT_READ_RSP 0x0b |
| ATT Read Response. This method is passed as a GATT message defined as attReadRsp_t. | |
| #define | ATT_SIGNED_WRITE_CMD 0xD2 |
| ATT Signed Write Command. | |
| #define | ATT_UNSUPPORTED_METHOD 0x20 |
| Garbage ATT opcode used for negative testing. | |
| #define | ATT_WRITE_CMD 0x52 |
| ATT Write Command. | |
| #define | ATT_WRITE_REQ 0x12 |
| ATT Write Request. This method is passed as a GATT message defined as attWriteReq_t. | |
| #define | ATT_WRITE_RSP 0x13 |
| ATT Write Response. This method is passed as a GATT message. | |