Data Structures | |
| struct | zb_zdo_nwk_addr_req_s |
| NWK_addr_req command primitive. More... | |
| struct | zb_zdo_nwk_addr_req_param_s |
| Parameters for nwk_addr_req command. More... | |
| struct | zb_zdo_nwk_addr_resp_head_s |
| NWK_addr_req response frame. More... | |
| struct | zb_zdo_nwk_addr_resp_ext_s |
| NWK_addr_req response frame tail. More... | |
| struct | zb_zdo_nwk_addr_resp_ext2_s |
| NWK_addr_req response frame tail. More... | |
| struct | zb_zdo_ieee_addr_req_s |
| Parameters of IEEE_addr_req primitive. More... | |
| struct | zb_zdo_ieee_addr_req_param_s |
| Parameters for ieee_addr_req command. More... | |
| struct | zb_zdo_ieee_addr_resp_s |
| struct | zb_zdo_ieee_addr_resp_ext_s |
| ZDO IEEE address response frame tail. More... | |
| struct | zb_zdo_ieee_addr_resp_ext2_s |
| ZDO IEEE address response frame tail. More... | |
Macros | |
| #define | ZB_ZDO_SINGLE_DEVICE_RESP 0U |
| #define | ZB_ZDO_EXTENDED_DEVICE_RESP 1U |
Functions | |
| zb_uint8_t | zb_zdo_nwk_addr_req (zb_uint8_t param, zb_callback_t cb) |
| Sends NWK_addr_req primitive. More... | |
| zb_uint8_t | zb_zdo_ieee_addr_req (zb_uint8_t param, zb_callback_t cb) |
| IEEE_addr_req primitive. More... | |
| #define ZB_ZDO_EXTENDED_DEVICE_RESP 1U |
Request Type parameter value of zb_zdo_nwk_addr_req_t and zb_zdo_ieee_addr_req_t for receiving an Extended device response used in the following commands accordingly:
| #define ZB_ZDO_SINGLE_DEVICE_RESP 0U |
Request Type parameter value of zb_zdo_nwk_addr_req_t and zb_zdo_ieee_addr_req_t for receiving a Single device response used in the following commands accordingly:
| typedef struct zb_zdo_ieee_addr_req_param_s zb_zdo_ieee_addr_req_param_t |
Parameters for ieee_addr_req command.
| typedef struct zb_zdo_ieee_addr_req_s zb_zdo_ieee_addr_req_t |
Parameters of IEEE_addr_req primitive.
To be put into buffer as data (means - after space alloc).
| typedef struct zb_zdo_ieee_addr_resp_ext2_s zb_zdo_ieee_addr_resp_ext2_t |
ZDO IEEE address response frame tail.
| typedef struct zb_zdo_ieee_addr_resp_ext_s zb_zdo_ieee_addr_resp_ext_t |
ZDO IEEE address response frame tail.
| typedef struct zb_zdo_ieee_addr_resp_s zb_zdo_ieee_addr_resp_t |
brief ZDO IEEE address response frame
| typedef struct zb_zdo_nwk_addr_req_param_s zb_zdo_nwk_addr_req_param_t |
Parameters for nwk_addr_req command.
| typedef struct zb_zdo_nwk_addr_req_s zb_zdo_nwk_addr_req_t |
NWK_addr_req command primitive.
| typedef struct zb_zdo_nwk_addr_resp_ext2_s zb_zdo_nwk_addr_resp_ext2_t |
NWK_addr_req response frame tail.
| typedef struct zb_zdo_nwk_addr_resp_ext_s zb_zdo_nwk_addr_resp_ext_t |
NWK_addr_req response frame tail.
| typedef struct zb_zdo_nwk_addr_resp_head_s zb_zdo_nwk_addr_resp_head_t |
NWK_addr_req response frame.
| zb_uint8_t zb_zdo_ieee_addr_req | ( | zb_uint8_t | param, |
| zb_callback_t | cb | ||
| ) |
IEEE_addr_req primitive.
| param | - index of buffer with primitive parameters zb_zdo_ieee_addr_req_s. Parameters must be put into the buffer as data (allocated). |
| cb | - user's function to call when got response from the remote. |
Example:
| zb_uint8_t zb_zdo_nwk_addr_req | ( | zb_uint8_t | param, |
| zb_callback_t | cb | ||
| ) |
Sends NWK_addr_req primitive.
| param | - index of buffer with primitive parameters - zb_zdo_nwk_addr_req_param_s |
| cb | - user's function to call when got response from the remote. zb_zdo_nwk_addr_resp_head_s passed to cb as parameter. |
Example: