Logo
Developing with ZBOSS for Zigbee
Metering cluster commands

Data Structures

struct  zb_zcl_metering_get_profile_payload_s
 
struct  zb_zcl_metering_get_profile_response_payload_s
 
struct  zb_zcl_metering_request_fast_poll_mode_payload_s
 
struct  zb_zcl_metering_request_fast_poll_mode_response_payload_s
 
struct  zb_zcl_metering_get_sampled_data_response_payload_s
 
struct  zb_zcl_metering_get_sampled_data_payload_s
 
struct  zb_zcl_metering_get_snapshot_payload_s
 
struct  zb_zcl_metering_tou_delivered_payload_s
 
struct  zb_zcl_metering_tou_received_payload_s
 
struct  zb_zcl_metering_block_delivered_payload_s
 
struct  zb_zcl_metering_block_received_payload_s
 
struct  zb_zcl_metering_tou_delivered_no_billing_payload_s
 
struct  zb_zcl_metering_tou_received_no_billing_payload_s
 
struct  zb_zcl_metering_block_tier_delivered_no_billing_payload_s
 
struct  zb_zcl_metering_block_tier_received_no_billing_payload_s
 
union  zb_zcl_metering_snapshot_sub_payload_s
 
struct  zb_zcl_metering_publish_snapshot_payload_s
 

Macros

#define ZB_ZCL_CLUSTER_ID_METERING_SERVER_ROLE_GENERATED_CMD_LIST
 
#define ZB_ZCL_CLUSTER_ID_METERING_CLIENT_ROLE_RECEIVED_CMD_LIST   ZB_ZCL_CLUSTER_ID_METERING_SERVER_ROLE_GENERATED_CMD_LIST
 
#define ZB_ZCL_CLUSTER_ID_METERING_CLIENT_ROLE_GENERATED_CMD_LIST
 
#define ZB_ZCL_CLUSTER_ID_METERING_SERVER_ROLE_RECEIVED_CMD_LIST   ZB_ZCL_CLUSTER_ID_METERING_CLIENT_ROLE_GENERATED_CMD_LIST
 
#define ZB_ZCL_METERING_GET_PROFILE_PAYLOAD_SIZE_IS_VALID(current_size)   ((current_size >= sizeof(zb_zcl_metering_get_profile_payload_t) ? ZB_TRUE : ZB_FALSE))
 
#define ZB_ZCL_METERING_SEND_CMD_GET_SNAPSHOT(_param, _dst_addr, _addr_mode, _dst_ep, _src_ep, _payload, cb)
 
#define ZB_ZCL_METERING_SEND_CMD_GET_SAMPLED_DATA(_param, _dst_addr, _addr_mode, _dst_ep, _src_ep, _payload, cb)
 
#define ZB_ZCL_METERING_SEND_CMD_REQUEST_FAST_POLL_MODE(_param, _dst_addr, _addr_mode, _dst_ep, _src_ep, _payload, cb)
 
#define ZB_ZCL_METERING_SEND_CMD_GET_PROFILE(_param, _dst_addr, _addr_mode, _dst_ep, _src_ep, _payload, cb)
 
#define ZB_ZCL_METERING_SEND_CMD_PUBLISH_SNAPSHOT(_param, _dst_addr, _addr_mode, _dst_ep, _src_ep, _payload, cb)
 
#define ZB_ZCL_METERING_SEND_CMD_REQUEST_FAST_POLL_MODE_RESPONSE(_param, _dst_addr, _addr_mode, _dst_ep, _src_ep, _payload, cb)
 
#define ZB_ZCL_METERING_SEND_CMD_GET_PROFILE_RESPONSE(_param, _dst_addr, _addr_mode, _dst_ep, _src_ep, _payload, _pl_size, cb)
 
#define ZB_ZCL_METERING_SEND_CMD_GET_SAMPLED_DATA_RESPONSE(_param, _dst_addr, _addr_mode, _dst_ep, _src_ep, _payload, _pl_size, cb)
 

Typedefs

typedef enum zb_zcl_metering_cli_cmd_e zb_zcl_metering_cli_cmd_t
 
typedef enum zb_zcl_metering_srv_cmd_e zb_zcl_metering_srv_cmd_t
 
typedef struct zb_zcl_metering_get_profile_payload_s zb_zcl_metering_get_profile_payload_t
 
typedef struct zb_zcl_metering_get_profile_response_payload_s zb_zcl_metering_get_profile_response_payload_t
 
typedef struct zb_zcl_metering_request_fast_poll_mode_payload_s zb_zcl_metering_request_fast_poll_mode_payload_t
 
typedef struct zb_zcl_metering_request_fast_poll_mode_response_payload_s zb_zcl_metering_request_fast_poll_mode_response_payload_t
 
typedef struct zb_zcl_metering_get_sampled_data_response_payload_s zb_zcl_metering_get_sampled_data_response_payload_t
 
typedef struct zb_zcl_metering_get_sampled_data_payload_s zb_zcl_metering_get_sampled_data_payload_t
 
typedef struct zb_zcl_metering_get_snapshot_payload_s zb_zcl_metering_get_snapshot_payload_t
 
typedef struct zb_zcl_metering_tou_delivered_payload_s zb_zcl_metering_tou_delivered_payload_t
 
typedef struct zb_zcl_metering_tou_received_payload_s zb_zcl_metering_tou_received_payload_t
 
typedef struct zb_zcl_metering_block_delivered_payload_s zb_zcl_metering_block_delivered_payload_t
 
typedef struct zb_zcl_metering_block_received_payload_s zb_zcl_metering_block_received_payload_t
 
typedef struct zb_zcl_metering_tou_delivered_no_billing_payload_s zb_zcl_metering_tou_delivered_no_billing_payload_t
 
typedef struct zb_zcl_metering_tou_received_no_billing_payload_s zb_zcl_metering_tou_received_no_billing_payload_t
 
typedef struct zb_zcl_metering_block_tier_delivered_no_billing_payload_s zb_zcl_metering_block_tier_delivered_no_billing_payload_t
 
typedef struct zb_zcl_metering_block_tier_received_no_billing_payload_s zb_zcl_metering_block_tier_received_no_billing_payload_t
 
typedef union zb_zcl_metering_snapshot_sub_payload_s zb_zcl_metering_snapshot_sub_payload_t
 
typedef struct zb_zcl_metering_publish_snapshot_payload_s zb_zcl_metering_publish_snapshot_payload_t
 

Enumerations

enum  zb_zcl_metering_cli_cmd_e {
  ZB_ZCL_METERING_CLI_CMD_GET_PROFILE = 0x00, ZB_ZCL_METERING_CLI_CMD_REQUEST_MIRROR_RESPONSE, ZB_ZCL_METERING_CLI_CMD_MIRROR_REMOVED, ZB_ZCL_METERING_CLI_CMD_REQUEST_FAST_POLL_MODE,
  ZB_ZCL_METERING_CLI_CMD_SCHEDULE_SNAPSHOT, ZB_ZCL_METERING_CLI_CMD_TAKE_SNAPSHOT, ZB_ZCL_METERING_CLI_CMD_GET_SNAPSHOT, ZB_ZCL_METERING_CLI_CMD_START_SAMPLING,
  ZB_ZCL_METERING_CLI_CMD_GET_SAMPLED_DATA, ZB_ZCL_METERING_CLI_CMD_MIRROR_REPORT_ATTRIBUTE_RESPONSE, ZB_ZCL_METERING_CLI_CMD_RESET_LOAD_LIMIT_COUNTER, ZB_ZCL_METERING_CLI_CMD_CHANGE_SUPPLY,
  ZB_ZCL_METERING_CLI_CMD_LOCAL_CHANGE_SUPPLY, ZB_ZCL_METERING_CLI_CMD_SET_SUPPLY_STATUS, ZB_ZCL_METERING_CLI_CMD_SET_UNCONTROLLED_FLOW_THRESHOLD
}
 
enum  zb_zcl_metering_srv_cmd_e {
  ZB_ZCL_METERING_SRV_CMD_GET_PROFILE_RESPONSE = 0x00, ZB_ZCL_METERING_SRV_CMD_REQUEST_MIRROR, ZB_ZCL_METERING_SRV_CMD_REMOVE_MIRROR, ZB_ZCL_METERING_SRV_CMD_REQUEST_FAST_POLL_MODE_RESPONSE,
  ZB_ZCL_METERING_SRV_CMD_SCHEDULE_SNAPSHOT_RESPONSE, ZB_ZCL_METERING_SRV_CMD_TAKE_SNAPSHOT_RESPONSE, ZB_ZCL_METERING_SRV_CMD_PUBLISH_SNAPSHOT, ZB_ZCL_METERING_SRV_CMD_GET_SAMPLED_DATA_RESPONSE,
  ZB_ZCL_METERING_SRV_CMD_CONFIGURE_MIRROR, ZB_ZCL_METERING_SRV_CMD_CONFIGURE_NOTIFICATION_SCHEME, ZB_ZCL_METERING_SRV_CMD_CONFIGURE_NOTIFICATION_FLAG, ZB_ZCL_METERING_SRV_CMD_GET_NOTIFIED_MESSAGE,
  ZB_ZCL_METERING_SRV_CMD_SUPPLY_STATUS_RESPONSE, ZB_ZCL_METERING_SRV_CMD_START_SAMPLING_RESPONSE
}
 
enum  zb_zcl_metering_interval_channel_e { ZB_ZCL_METERING_CONSUMPTION_DELIVERED = 0, ZB_ZCL_METERING_CONSUMPTION_RECEIVED = 1, ZB_ZCL_METERING_REACTIVE_CONSUMPTION_DELIVERED = 2, ZB_ZCL_METERING_REACTIVE_CONSUMPTION_RECEIVED = 3 }
 
enum  zb_zcl_metering_status_field_e {
  ZB_ZCL_METERING_SUCCESS = 0x00, ZB_ZCL_METERING_UNDEFINED_INTERVAL_CHANNEL_REQUESTED = 0x01, ZB_ZCL_METERING_INTERVAL_CHANNEL_NOT_SUPPORTED = 0x02, ZB_ZCL_METERING_INVALID_END_TIME = 0x03,
  ZB_ZCL_METERING_MORE_PERIODS_REQUESTED_THAN_CAN_BE_RETURNED = 0x04, ZB_ZCL_METERING_NO_INTERVALS_AVAILABLE_FOR_THE_REQUESTED_TIME = 0x05
}
 
enum  zb_zcl_metering_profile_interval_period_e {
  ZB_ZCl_METERING_INTERVAL_PERIOD_DAILY = 0, ZB_ZCl_METERING_INTERVAL_PERIOD_60_MINUTES = 1, ZB_ZCl_METERING_INTERVAL_PERIOD_30_MINUTES = 2, ZB_ZCl_METERING_INTERVAL_PERIOD_15_MINUTES = 3,
  ZB_ZCl_METERING_INTERVAL_PERIOD_10_MINUTES = 4, ZB_ZCl_METERING_INTERVAL_PERIOD_7_5_MINUTES = 5, ZB_ZCl_METERING_INTERVAL_PERIOD_5_MINUTES = 6, ZB_ZCl_METERING_INTERVAL_PERIOD_2_5_MINUTES = 7,
  ZB_ZCl_METERING_INTERVAL_PERIOD_1_MINUTE = 8
}
 
enum  zb_zcl_metering_sample_type_e {
  ZB_ZCL_METERING_SAMPLE_TYPE_CONSUMPTION_DELIVERED = 0, ZB_ZCL_METERING_SAMPLE_TYPE_CONSUMPTION_RECEIVED = 1, ZB_ZCL_METERING_SAMPLE_TYPE_REACTIVE_CONSUMPTION_DELIVERED = 2, ZB_ZCL_METERING_SAMPLE_TYPE_REACTIVE_CONSUMPTION_RECEIVED = 3,
  ZB_ZCL_METERING_SAMPLE_TYPE_INSTANTANEOUS_DEMAND = 4
}
 
enum  zb_zcl_metering_snapshot_cause_e {
  ZB_ZCL_METERING_CAUSE_GENERAL = 1 << 0, ZB_ZCL_METERING_CAUSE_END_OF_BILLING_PERIOD = 1 << 1, ZB_ZCL_METERING_CAUSE_END_OF_BLOCK_PERIOD = 1 << 2, ZB_ZCL_METERING_CAUSE_CHANGE_OF_TARIFF_INFORMATION = 1 << 3,
  ZB_ZCL_METERING_CAUSE_CHANGE_OF_PRICE_MATRIX = 1 << 4, ZB_ZCL_METERING_CAUSE_CHANGE_OF_BLOCK_THRESHOLDS = 1 << 5, ZB_ZCL_METERING_CAUSE_CHANGE_OF_CV = 1 << 6, ZB_ZCL_METERING_CAUSE_CHANGE_OF_CF = 1 << 7,
  ZB_ZCL_METERING_CAUSE_CHANGE_OF_CALENDAR = 1 << 8, ZB_ZCL_METERING_CAUSE_CRITICAL_PEAK_PRICING = 1 << 9, ZB_ZCL_METERING_CAUSE_MANUALLY_TRIGGERED_FROM_CLIENT = 1 << 10, ZB_ZCL_METERING_CAUSE_END_OF_RESOLVE_PERIOD = 1 << 11,
  ZB_ZCL_METERING_CAUSE_CHANGE_OF_TENANCY = 1 << 12, ZB_ZCL_METERING_CAUSE_CHANGE_OF_SUPPLIER = 1 << 13, ZB_ZCL_METERING_CAUSE_CHANGE_OF_METER_MODE = 1 << 14, ZB_ZCL_METERING_CAUSE_DEBT_PAYMENT = 1 << 15,
  ZB_ZCL_METERING_CAUSE_SCHEDULED_SNAPSHOT = 1 << 16, ZB_ZCL_METERING_CAUSE_OTA_FIRMWARE_DOWNLOAD = 1 << 17, ZB_ZCL_METERING_CAUSE_SELECT_ALL_SNAPSHOTS = 0xFFFFFFFF
}
 
enum  zb_zcl_metering_snapshot_payload_type_e {
  ZB_ZCL_METERING_TOU_DELIVERED_REGISTERS = 0, ZB_ZCL_METERING_TOU_RECEIVED_REGISTERS = 1, ZB_ZCL_METERING_BLOCK_TIER_DELIVERED = 2, ZB_ZCL_METERING_BLOCK_TIER_RECEIVED = 3,
  ZB_ZCL_METERING_TOU_DELIVERED_NO_BILLING = 4, ZB_ZCL_METERING_TOU_RECEIVED_NO_BILLING = 5, ZB_ZCL_METERING_BLOCK_TIER_DELIVERED_NO_BILLING = 6, ZB_ZCL_METERING_BLOCK_TIER_RECEIVED_NO_BILLING = 7,
  ZB_ZCL_METERING_DATA_UNAVAILABLE = 128
}
 

Functions

void zb_zcl_metering_send_cmd_get_snapshot (zb_uint8_t param, zb_addr_u *dst_addr, zb_aps_addr_mode_t dst_addr_mode, zb_uint8_t dst_ep, zb_uint8_t src_ep, zb_zcl_metering_get_snapshot_payload_t *payload, zb_callback_t cb)
 
void zb_zcl_metering_send_cmd_get_sampled_data (zb_uint8_t param, zb_addr_u *dst_addr, zb_aps_addr_mode_t dst_addr_mode, zb_uint8_t dst_ep, zb_uint8_t src_ep, zb_zcl_metering_get_sampled_data_payload_t *payload, zb_callback_t cb)
 
void zb_zcl_metering_send_cmd_request_fast_poll_mode (zb_uint8_t param, zb_addr_u *dst_addr, zb_aps_addr_mode_t dst_addr_mode, zb_uint8_t dst_ep, zb_uint8_t src_ep, zb_zcl_metering_request_fast_poll_mode_payload_t *payload, zb_callback_t cb)
 
void zb_zcl_metering_send_cmd_get_profile (zb_uint8_t param, zb_addr_u *dst_addr, zb_aps_addr_mode_t dst_addr_mode, zb_uint8_t dst_ep, zb_uint8_t src_ep, zb_zcl_metering_get_profile_payload_t *payload, zb_callback_t cb)
 
void zb_zcl_metering_send_cmd_publish_snapshot (zb_uint8_t param, const zb_addr_u *dst_addr, zb_aps_addr_mode_t dst_addr_mode, zb_uint8_t dst_ep, zb_uint8_t src_ep, const zb_zcl_metering_publish_snapshot_payload_t *pl, zb_callback_t cb)
 
void zb_zcl_metering_send_cmd_request_fast_poll_mode_response (zb_uint8_t param, const zb_addr_u *dst_addr, zb_aps_addr_mode_t dst_addr_mode, zb_uint8_t dst_ep, zb_uint8_t src_ep, const zb_zcl_metering_request_fast_poll_mode_response_payload_t *pl, zb_uint8_t pl_size, zb_uint8_t tsn, zb_callback_t cb)
 
void zb_zcl_metering_send_cmd_get_profile_response (zb_uint8_t param, const zb_addr_u *dst_addr, zb_aps_addr_mode_t dst_addr_mode, zb_uint8_t dst_ep, zb_uint8_t src_ep, const zb_zcl_metering_get_profile_response_payload_t *pl, zb_uint8_t pl_size, zb_uint8_t tsn, zb_callback_t cb)
 
void zb_zcl_metering_send_cmd_get_sampled_data_response (zb_uint8_t param, const zb_addr_u *dst_addr, zb_aps_addr_mode_t dst_addr_mode, zb_uint8_t dst_ep, zb_uint8_t src_ep, const zb_zcl_metering_get_sampled_data_response_payload_t *pl, zb_uint8_t pl_size, zb_uint8_t tsn, zb_callback_t cb)
 

Detailed Description

Macro Definition Documentation

§ ZB_ZCL_CLUSTER_ID_METERING_CLIENT_ROLE_GENERATED_CMD_LIST

#define ZB_ZCL_CLUSTER_ID_METERING_CLIENT_ROLE_GENERATED_CMD_LIST

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Value:
ZB_ZCL_METERING_CLI_CMD_REQUEST_FAST_POLL_MODE, \
ZB_ZCL_METERING_CLI_CMD_GET_SNAPSHOT, \
ZB_ZCL_METERING_CLI_CMD_GET_SAMPLED_DATA
Definition: zb_zcl_metering.h:1383

§ ZB_ZCL_CLUSTER_ID_METERING_CLIENT_ROLE_RECEIVED_CMD_LIST

§ ZB_ZCL_CLUSTER_ID_METERING_SERVER_ROLE_GENERATED_CMD_LIST

#define ZB_ZCL_CLUSTER_ID_METERING_SERVER_ROLE_GENERATED_CMD_LIST

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Value:
ZB_ZCL_METERING_SRV_CMD_REQUEST_FAST_POLL_MODE_RESPONSE, \
ZB_ZCL_METERING_SRV_CMD_PUBLISH_SNAPSHOT, \
ZB_ZCL_METERING_SRV_CMD_GET_SAMPLED_DATA_RESPONSE
Definition: zb_zcl_metering.h:1459

§ ZB_ZCL_CLUSTER_ID_METERING_SERVER_ROLE_RECEIVED_CMD_LIST

§ ZB_ZCL_METERING_GET_PROFILE_PAYLOAD_SIZE_IS_VALID

§ ZB_ZCL_METERING_SEND_CMD_GET_PROFILE

#define ZB_ZCL_METERING_SEND_CMD_GET_PROFILE (   _param,
  _dst_addr,
  _addr_mode,
  _dst_ep,
  _src_ep,
  _payload,
  cb 
)

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Value:
zb_zcl_metering_send_cmd_get_profile(_param, _dst_addr, _addr_mode, \
_dst_ep, _src_ep, _payload, cb)
void zb_zcl_metering_send_cmd_get_profile(zb_uint8_t param, zb_addr_u *dst_addr, zb_aps_addr_mode_t dst_addr_mode, zb_uint8_t dst_ep, zb_uint8_t src_ep, zb_zcl_metering_get_profile_payload_t *payload, zb_callback_t cb)

Macro for call zb_zcl_metering_send_cmd_get_profile function

§ ZB_ZCL_METERING_SEND_CMD_GET_PROFILE_RESPONSE

#define ZB_ZCL_METERING_SEND_CMD_GET_PROFILE_RESPONSE (   _param,
  _dst_addr,
  _addr_mode,
  _dst_ep,
  _src_ep,
  _payload,
  _pl_size,
  cb 
)

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Value:
zb_zcl_metering_send_cmd_get_profile_response(_param, _dst_addr, _addr_mode, _dst_ep, \
_src_ep, _payload, _pl_size, cb)
void zb_zcl_metering_send_cmd_get_profile_response(zb_uint8_t param, const zb_addr_u *dst_addr, zb_aps_addr_mode_t dst_addr_mode, zb_uint8_t dst_ep, zb_uint8_t src_ep, const zb_zcl_metering_get_profile_response_payload_t *pl, zb_uint8_t pl_size, zb_uint8_t tsn, zb_callback_t cb)

Macro for call zb_zcl_metering_send_cmd_get_profile_response function

§ ZB_ZCL_METERING_SEND_CMD_GET_SAMPLED_DATA

#define ZB_ZCL_METERING_SEND_CMD_GET_SAMPLED_DATA (   _param,
  _dst_addr,
  _addr_mode,
  _dst_ep,
  _src_ep,
  _payload,
  cb 
)

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Value:
zb_zcl_metering_send_cmd_get_sampled_data(_param, _dst_addr, _addr_mode, \
_dst_ep, _src_ep, _payload, cb)
void zb_zcl_metering_send_cmd_get_sampled_data(zb_uint8_t param, zb_addr_u *dst_addr, zb_aps_addr_mode_t dst_addr_mode, zb_uint8_t dst_ep, zb_uint8_t src_ep, zb_zcl_metering_get_sampled_data_payload_t *payload, zb_callback_t cb)

Macro for call zb_zcl_metering_send_cmd_get_sampled_data function

§ ZB_ZCL_METERING_SEND_CMD_GET_SAMPLED_DATA_RESPONSE

#define ZB_ZCL_METERING_SEND_CMD_GET_SAMPLED_DATA_RESPONSE (   _param,
  _dst_addr,
  _addr_mode,
  _dst_ep,
  _src_ep,
  _payload,
  _pl_size,
  cb 
)

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Value:
zb_zcl_metering_send_cmd_get_sampled_data_response(_param, _dst_addr, _addr_mode, _dst_ep, \
_src_ep, _payload, _pl_size, cb)
void zb_zcl_metering_send_cmd_get_sampled_data_response(zb_uint8_t param, const zb_addr_u *dst_addr, zb_aps_addr_mode_t dst_addr_mode, zb_uint8_t dst_ep, zb_uint8_t src_ep, const zb_zcl_metering_get_sampled_data_response_payload_t *pl, zb_uint8_t pl_size, zb_uint8_t tsn, zb_callback_t cb)

Macro for call zb_zcl_metering_send_cmd_get_sampled_data_response function

§ ZB_ZCL_METERING_SEND_CMD_GET_SNAPSHOT

#define ZB_ZCL_METERING_SEND_CMD_GET_SNAPSHOT (   _param,
  _dst_addr,
  _addr_mode,
  _dst_ep,
  _src_ep,
  _payload,
  cb 
)

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Value:
zb_zcl_metering_send_cmd_get_snapshot(_param, _dst_addr, _addr_mode, \
_dst_ep, _src_ep, _payload, cb)
void zb_zcl_metering_send_cmd_get_snapshot(zb_uint8_t param, zb_addr_u *dst_addr, zb_aps_addr_mode_t dst_addr_mode, zb_uint8_t dst_ep, zb_uint8_t src_ep, zb_zcl_metering_get_snapshot_payload_t *payload, zb_callback_t cb)

Macro for call zb_zcl_metering_send_cmd_get_snapshot function

§ ZB_ZCL_METERING_SEND_CMD_PUBLISH_SNAPSHOT

#define ZB_ZCL_METERING_SEND_CMD_PUBLISH_SNAPSHOT (   _param,
  _dst_addr,
  _addr_mode,
  _dst_ep,
  _src_ep,
  _payload,
  cb 
)

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Value:
zb_zcl_metering_send_cmd_publish_snapshot(_param, _dst_addr, _addr_mode, \
_dst_ep, _src_ep, _payload, cb)
void zb_zcl_metering_send_cmd_publish_snapshot(zb_uint8_t param, const zb_addr_u *dst_addr, zb_aps_addr_mode_t dst_addr_mode, zb_uint8_t dst_ep, zb_uint8_t src_ep, const zb_zcl_metering_publish_snapshot_payload_t *pl, zb_callback_t cb)

Macro for call zb_zcl_metering_send_cmd_publish_snapshot function

§ ZB_ZCL_METERING_SEND_CMD_REQUEST_FAST_POLL_MODE

#define ZB_ZCL_METERING_SEND_CMD_REQUEST_FAST_POLL_MODE (   _param,
  _dst_addr,
  _addr_mode,
  _dst_ep,
  _src_ep,
  _payload,
  cb 
)

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Value:
zb_zcl_metering_send_cmd_request_fast_poll_mode(_param, _dst_addr, _addr_mode, \
_dst_ep, _src_ep, _payload, cb)
void zb_zcl_metering_send_cmd_request_fast_poll_mode(zb_uint8_t param, zb_addr_u *dst_addr, zb_aps_addr_mode_t dst_addr_mode, zb_uint8_t dst_ep, zb_uint8_t src_ep, zb_zcl_metering_request_fast_poll_mode_payload_t *payload, zb_callback_t cb)

Macro for call zb_zcl_metering_send_cmd_request_fast_poll_mode function

§ ZB_ZCL_METERING_SEND_CMD_REQUEST_FAST_POLL_MODE_RESPONSE

#define ZB_ZCL_METERING_SEND_CMD_REQUEST_FAST_POLL_MODE_RESPONSE (   _param,
  _dst_addr,
  _addr_mode,
  _dst_ep,
  _src_ep,
  _payload,
  cb 
)

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Value:
_dst_ep, _src_ep, _payload, cb)
void zb_zcl_metering_send_cmd_request_fast_poll_mode_response(zb_uint8_t param, const zb_addr_u *dst_addr, zb_aps_addr_mode_t dst_addr_mode, zb_uint8_t dst_ep, zb_uint8_t src_ep, const zb_zcl_metering_request_fast_poll_mode_response_payload_t *pl, zb_uint8_t pl_size, zb_uint8_t tsn, zb_callback_t cb)

Macro for call zb_zcl_metering_send_cmd_request_fast_poll_mode_response function

Typedef Documentation

§ zb_zcl_metering_block_delivered_payload_t

§ zb_zcl_metering_block_received_payload_t

§ zb_zcl_metering_block_tier_delivered_no_billing_payload_t

§ zb_zcl_metering_block_tier_received_no_billing_payload_t

§ zb_zcl_metering_cli_cmd_t

§ zb_zcl_metering_get_profile_payload_t

§ zb_zcl_metering_get_profile_response_payload_t

§ zb_zcl_metering_get_sampled_data_payload_t

§ zb_zcl_metering_get_sampled_data_response_payload_t

§ zb_zcl_metering_get_snapshot_payload_t

§ zb_zcl_metering_publish_snapshot_payload_t

§ zb_zcl_metering_request_fast_poll_mode_payload_t

§ zb_zcl_metering_request_fast_poll_mode_response_payload_t

§ zb_zcl_metering_snapshot_sub_payload_t

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

The format of the Snapshot Sub-Payload differs depending on the SnapshotPayloadType

See also
SE spec, Table D-53 and D.3.2.3.1.7

§ zb_zcl_metering_srv_cmd_t

§ zb_zcl_metering_tou_delivered_no_billing_payload_t

§ zb_zcl_metering_tou_delivered_payload_t

§ zb_zcl_metering_tou_received_no_billing_payload_t

§ zb_zcl_metering_tou_received_payload_t

Enumeration Type Documentation

§ zb_zcl_metering_cli_cmd_e

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Metering cluster client command identifiers.

See also
SE spec, subclause D.3.3.3.1
Enumerator
ZB_ZCL_METERING_CLI_CMD_GET_PROFILE 

GetProfile command

ZB_ZCL_METERING_CLI_CMD_REQUEST_MIRROR_RESPONSE 

The RequestMirrorResponse command allows the ESI to inform a sleepy Metering Device it has the ability to store and mirror its data.

ZB_ZCL_METERING_CLI_CMD_MIRROR_REMOVED 

The MirrorRemovedCommand allows the ESI to inform a sleepy Metering Device mirroring support has been removed or halted.

ZB_ZCL_METERING_CLI_CMD_REQUEST_FAST_POLL_MODE 

RequestFastPollMode command

ZB_ZCL_METERING_CLI_CMD_SCHEDULE_SNAPSHOT 

This command is used to set up a schedule of when the device shall create snapshot data.

ZB_ZCL_METERING_CLI_CMD_TAKE_SNAPSHOT 

This command is used to instruct the cluster server to take a single snapshot.

ZB_ZCL_METERING_CLI_CMD_GET_SNAPSHOT 

This command is used to request snapshot data from the cluster server.

ZB_ZCL_METERING_CLI_CMD_START_SAMPLING 

The sampling mechanism allows a set of samples of the specified type of data to be taken, commencing at the stipulated start time.

ZB_ZCL_METERING_CLI_CMD_GET_SAMPLED_DATA 

This command is used to request sampled data from the server.

ZB_ZCL_METERING_CLI_CMD_MIRROR_REPORT_ATTRIBUTE_RESPONSE 

This command is sent in response to the ReportAttribute command when the MirrorReporting attribute is set.

ZB_ZCL_METERING_CLI_CMD_RESET_LOAD_LIMIT_COUNTER 

The ResetLoadLimitCounter command shall cause the LoadLimitCounter attribute to be reset

ZB_ZCL_METERING_CLI_CMD_CHANGE_SUPPLY 

This command is sent from the Head-end or ESI to the Metering Device to instruct it to change the status of the valve or load switch, i.e. the supply.

ZB_ZCL_METERING_CLI_CMD_LOCAL_CHANGE_SUPPLY 

This command is a simplified version of the Change Supply command, intended to be sent from an IHD to a meter as the consequence of a user action on the IHD.

ZB_ZCL_METERING_CLI_CMD_SET_SUPPLY_STATUS 

This command is used to specify the required status of the supply following the occurrence of certain events on the meter.

ZB_ZCL_METERING_CLI_CMD_SET_UNCONTROLLED_FLOW_THRESHOLD 

This command is used to update the 'Uncontrolled Flow Rate' configuration data used by flow meters.

§ zb_zcl_metering_interval_channel_e

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Interval Channel Values

See also
SE spec, subclause D.3.3.3.1.1.1
Enumerator
ZB_ZCL_METERING_CONSUMPTION_DELIVERED 
ZB_ZCL_METERING_CONSUMPTION_RECEIVED 
ZB_ZCL_METERING_REACTIVE_CONSUMPTION_DELIVERED 
ZB_ZCL_METERING_REACTIVE_CONSUMPTION_RECEIVED 

§ zb_zcl_metering_profile_interval_period_e

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Profile Interval Period

See also
SE spec, Table D-49
Enumerator
ZB_ZCl_METERING_INTERVAL_PERIOD_DAILY 

Daily

ZB_ZCl_METERING_INTERVAL_PERIOD_60_MINUTES 

60 minutes

ZB_ZCl_METERING_INTERVAL_PERIOD_30_MINUTES 

30 minutes

ZB_ZCl_METERING_INTERVAL_PERIOD_15_MINUTES 

15 minutes

ZB_ZCl_METERING_INTERVAL_PERIOD_10_MINUTES 

10 minutes

ZB_ZCl_METERING_INTERVAL_PERIOD_7_5_MINUTES 

7.5 minutes

ZB_ZCl_METERING_INTERVAL_PERIOD_5_MINUTES 

5 minutes

ZB_ZCl_METERING_INTERVAL_PERIOD_2_5_MINUTES 

2.5 minutes

ZB_ZCl_METERING_INTERVAL_PERIOD_1_MINUTE 

1 minute

§ zb_zcl_metering_sample_type_e

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Sample Type Enumerations

See also
SE spec, Table D-54
Enumerator
ZB_ZCL_METERING_SAMPLE_TYPE_CONSUMPTION_DELIVERED 

Consumption Delivered

ZB_ZCL_METERING_SAMPLE_TYPE_CONSUMPTION_RECEIVED 

Consumption Received

ZB_ZCL_METERING_SAMPLE_TYPE_REACTIVE_CONSUMPTION_DELIVERED 

Reactive Consumption Delivered

ZB_ZCL_METERING_SAMPLE_TYPE_REACTIVE_CONSUMPTION_RECEIVED 

Reactive Consumption Received

ZB_ZCL_METERING_SAMPLE_TYPE_INSTANTANEOUS_DEMAND 

InstantaneousDemand

§ zb_zcl_metering_snapshot_cause_e

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Snapshot Cause BitMap

See also
SE spec, Table D-52
Enumerator
ZB_ZCL_METERING_CAUSE_GENERAL 

General

ZB_ZCL_METERING_CAUSE_END_OF_BILLING_PERIOD 

End of Billing Period

ZB_ZCL_METERING_CAUSE_END_OF_BLOCK_PERIOD 

End of Block Period

ZB_ZCL_METERING_CAUSE_CHANGE_OF_TARIFF_INFORMATION 

Change of Tariff Information

ZB_ZCL_METERING_CAUSE_CHANGE_OF_PRICE_MATRIX 

Change of Price Matrix

ZB_ZCL_METERING_CAUSE_CHANGE_OF_BLOCK_THRESHOLDS 

Change of Block Thresholds

ZB_ZCL_METERING_CAUSE_CHANGE_OF_CV 

Change of CV

ZB_ZCL_METERING_CAUSE_CHANGE_OF_CF 

Change of CF

ZB_ZCL_METERING_CAUSE_CHANGE_OF_CALENDAR 

Change of Calendar

ZB_ZCL_METERING_CAUSE_CRITICAL_PEAK_PRICING 

Critical Peak Pricing

ZB_ZCL_METERING_CAUSE_MANUALLY_TRIGGERED_FROM_CLIENT 

Manually Triggered from Client

ZB_ZCL_METERING_CAUSE_END_OF_RESOLVE_PERIOD 

End of Resolve Period

ZB_ZCL_METERING_CAUSE_CHANGE_OF_TENANCY 

Change of Tenancy

ZB_ZCL_METERING_CAUSE_CHANGE_OF_SUPPLIER 

Change of Supplier

ZB_ZCL_METERING_CAUSE_CHANGE_OF_METER_MODE 

Change of (Meter) Mode

ZB_ZCL_METERING_CAUSE_DEBT_PAYMENT 

Debt Payment

ZB_ZCL_METERING_CAUSE_SCHEDULED_SNAPSHOT 

Scheduled Snapshot

ZB_ZCL_METERING_CAUSE_OTA_FIRMWARE_DOWNLOAD 

OTA Firmware Download

ZB_ZCL_METERING_CAUSE_SELECT_ALL_SNAPSHOTS 

Select All Snapshots

§ zb_zcl_metering_snapshot_payload_type_e

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Snapshot Payload Type

See also
SE spec, Table D-53
Enumerator
ZB_ZCL_METERING_TOU_DELIVERED_REGISTERS 

TOU Information Set DeliveredRegisters

ZB_ZCL_METERING_TOU_RECEIVED_REGISTERS 

TOU Information Set Received Registers

ZB_ZCL_METERING_BLOCK_TIER_DELIVERED 

Block Tier Information Set Delivered

ZB_ZCL_METERING_BLOCK_TIER_RECEIVED 

Block Tier Information Set Received

ZB_ZCL_METERING_TOU_DELIVERED_NO_BILLING 

TOU Information Set Delivered (No Billing)

ZB_ZCL_METERING_TOU_RECEIVED_NO_BILLING 

TOU Information Set Received (No Billing)

ZB_ZCL_METERING_BLOCK_TIER_DELIVERED_NO_BILLING 

Block Tier Information Set Delivered (No Billing)

ZB_ZCL_METERING_BLOCK_TIER_RECEIVED_NO_BILLING 

Block Tier Information Set Received (No Billing)

ZB_ZCL_METERING_DATA_UNAVAILABLE 

Data Unavailable

§ zb_zcl_metering_srv_cmd_e

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Metering cluster server command identifiers.

See also
SE spec, D.3.2.3.1
Enumerator
ZB_ZCL_METERING_SRV_CMD_GET_PROFILE_RESPONSE 

Get Profile Response

ZB_ZCL_METERING_SRV_CMD_REQUEST_MIRROR 

This command is used to request the ESI to mirror Metering Device data.

ZB_ZCL_METERING_SRV_CMD_REMOVE_MIRROR 

This command is used to request the ESI to remove its mirror of Metering Device data.

ZB_ZCL_METERING_SRV_CMD_REQUEST_FAST_POLL_MODE_RESPONSE 

RequestFastPollModeResponse command

ZB_ZCL_METERING_SRV_CMD_SCHEDULE_SNAPSHOT_RESPONSE 

This command is generated in response to a ScheduleSnapshot command, and is sent to confirm whether the requested snapshot schedule has been set up.

ZB_ZCL_METERING_SRV_CMD_TAKE_SNAPSHOT_RESPONSE 

This command is generated in response to a TakeSnapshot command, and is sent to confirm whether the requested snapshot has been accepted and successfully taken.

ZB_ZCL_METERING_SRV_CMD_PUBLISH_SNAPSHOT 

This command is generated in response to a GetSnapshot command or when a new snapshot is created.

ZB_ZCL_METERING_SRV_CMD_GET_SAMPLED_DATA_RESPONSE 

This command is used to send the requested sample data to the client. It is generated in response to a GetSampledData command

ZB_ZCL_METERING_SRV_CMD_CONFIGURE_MIRROR 

Where 'Two Way Mirroring' is being implemented, this command shall be sent to the mirror once the mirror has been created. The command allows a BOMD to provide the operational configuration of the associated Mirror.

ZB_ZCL_METERING_SRV_CMD_CONFIGURE_NOTIFICATION_SCHEME 

Where 'Two Way Mirroring' is being implemented, and a non-default Notification Scheme is to be used, this command shall be sent to the mirror once the mirror has been created.

ZB_ZCL_METERING_SRV_CMD_CONFIGURE_NOTIFICATION_FLAG 

Where 'Two Way Mirroring' is being implemented, and a non-default Notification Scheme is to be used, the ConfigureNotificationFlags command allows a BOMD to set the commands relating to the bit value for each NotificationFlags::N attribute that the scheme is proposing to use.

ZB_ZCL_METERING_SRV_CMD_GET_NOTIFIED_MESSAGE 

The GetNotifiedMessage command is used only when a BOMD is being mirrored. This command provides a method for the BOMD to notify the Mirror message queue that it wants to receive commands that the Mirror has queued.

ZB_ZCL_METERING_SRV_CMD_SUPPLY_STATUS_RESPONSE 

This command is transmitted by a Metering Device in response to a Change Supply command.

ZB_ZCL_METERING_SRV_CMD_START_SAMPLING_RESPONSE 

This command is transmitted by a Metering Device in response to a StartSampling command.

§ zb_zcl_metering_status_field_e

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Status Field Values

See also
SE spec, Table D-48
Enumerator
ZB_ZCL_METERING_SUCCESS 

Success

ZB_ZCL_METERING_UNDEFINED_INTERVAL_CHANNEL_REQUESTED 

Undefined Interval Channel requested

ZB_ZCL_METERING_INTERVAL_CHANNEL_NOT_SUPPORTED 

Interval Channel not supported

ZB_ZCL_METERING_INVALID_END_TIME 

Invalid End Time

ZB_ZCL_METERING_MORE_PERIODS_REQUESTED_THAN_CAN_BE_RETURNED 

More periods requested than can be returned

ZB_ZCL_METERING_NO_INTERVALS_AVAILABLE_FOR_THE_REQUESTED_TIME 

No intervals available for the requested time

Function Documentation

§ zb_zcl_metering_send_cmd_get_profile()

void zb_zcl_metering_send_cmd_get_profile ( zb_uint8_t  param,
zb_addr_u dst_addr,
zb_aps_addr_mode_t  dst_addr_mode,
zb_uint8_t  dst_ep,
zb_uint8_t  src_ep,
zb_zcl_metering_get_profile_payload_t payload,
zb_callback_t  cb 
)

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Function for send GetProfile command. On receiver's side callback ZCL device callback ZB_ZCL_REGISTER_DEVICE_CB will be called with ZB_ZCL_METERING_GET_PROFILE_CB_ID

Parameters
param- Reference to buffer.
dst_addr- Address of the device to send command to.
dst_addr_mode- Address mode for dst_addr.
dst_ep- Destination endpoint.
src_ep- Current endpoint.
payload- Packet payload (ref to zb_zcl_metering_get_profile_payload_t).
cb- Callback which should be called when the ZCL stack receives APS ack.

§ zb_zcl_metering_send_cmd_get_profile_response()

void zb_zcl_metering_send_cmd_get_profile_response ( zb_uint8_t  param,
const zb_addr_u dst_addr,
zb_aps_addr_mode_t  dst_addr_mode,
zb_uint8_t  dst_ep,
zb_uint8_t  src_ep,
const zb_zcl_metering_get_profile_response_payload_t pl,
zb_uint8_t  pl_size,
zb_uint8_t  tsn,
zb_callback_t  cb 
)

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Function for send GetProfileResponse command. On receiver's side callback ZCL device callback ZB_ZCL_REGISTER_DEVICE_CB will be called with ZB_ZCL_METERING_GET_PROFILE_RESPONSE_CB_ID

Parameters
param- Reference to buffer.
dst_addr- Address of the device to send command to.
dst_addr_mode- Address mode for dst_addr.
dst_ep- Destination endpoint.
src_ep- Current endpoint.
pl- Packet payload (ref to zb_zcl_metering_get_profile_response_payload_t).
pl_size- size in bytes of input payload. Stack can calculate actual payload size. Set pl_size to 0 for it.
tsn- transaction sequence number of response
cb- Callback which should be called when the ZCL stack receives APS ack.

§ zb_zcl_metering_send_cmd_get_sampled_data()

void zb_zcl_metering_send_cmd_get_sampled_data ( zb_uint8_t  param,
zb_addr_u dst_addr,
zb_aps_addr_mode_t  dst_addr_mode,
zb_uint8_t  dst_ep,
zb_uint8_t  src_ep,
zb_zcl_metering_get_sampled_data_payload_t payload,
zb_callback_t  cb 
)

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Function for send GetSampledData command. On receiver's side callback ZCL device callback ZB_ZCL_REGISTER_DEVICE_CB will be called with ZB_ZCL_METERING_GET_SAMPLED_DATA_CB_ID

Parameters
param- Reference to buffer.
dst_addr- Address of the device to send command to.
dst_addr_mode- Address mode for dst_addr.
dst_ep- Destination endpoint.
src_ep- Current endpoint.
payload- Packet payload (ref to zb_zcl_metering_get_sampled_data_payload_t).
cb- Callback which should be called when the ZCL stack receives APS ack.

§ zb_zcl_metering_send_cmd_get_sampled_data_response()

void zb_zcl_metering_send_cmd_get_sampled_data_response ( zb_uint8_t  param,
const zb_addr_u dst_addr,
zb_aps_addr_mode_t  dst_addr_mode,
zb_uint8_t  dst_ep,
zb_uint8_t  src_ep,
const zb_zcl_metering_get_sampled_data_response_payload_t pl,
zb_uint8_t  pl_size,
zb_uint8_t  tsn,
zb_callback_t  cb 
)

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Function for send GetSampledDataResponse command. On receiver's side callback ZCL device callback ZB_ZCL_REGISTER_DEVICE_CB will be called with ZB_ZCL_METERING_GET_SAMPLED_DATA_RESPONSE_CB_ID

Parameters
param- Reference to buffer.
dst_addr- Address of the device to send command to.
dst_addr_mode- Address mode for dst_addr.
dst_ep- Destination endpoint.
src_ep- Current endpoint.
pl- Packet payload (ref to zb_zcl_metering_get_sampled_data_response_payload_t).
pl_size- size in bytes of input payload. Stack can calculate actual payload size. Set pl_size to 0 for it.
tsn- transaction sequence number of response
cb- Callback which should be called when the ZCL stack receives APS ack.

§ zb_zcl_metering_send_cmd_get_snapshot()

void zb_zcl_metering_send_cmd_get_snapshot ( zb_uint8_t  param,
zb_addr_u dst_addr,
zb_aps_addr_mode_t  dst_addr_mode,
zb_uint8_t  dst_ep,
zb_uint8_t  src_ep,
zb_zcl_metering_get_snapshot_payload_t payload,
zb_callback_t  cb 
)

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Function for send GetSnapshot command. On receiver's side callback ZCL device callback ZB_ZCL_REGISTER_DEVICE_CB will be called with ZB_ZCL_METERING_GET_SNAPSHOT_CB_ID

Parameters
param- Reference to buffer.
dst_addr- Address of the device to send command to.
dst_addr_mode- Address mode for dst_addr.
dst_ep- Destination endpoint.
src_ep- Current endpoint.
payload- Packet payload (ref to zb_zcl_metering_get_snapshot_payload_t).
cb- Callback which should be called when the ZCL stack receives APS ack.

§ zb_zcl_metering_send_cmd_publish_snapshot()

void zb_zcl_metering_send_cmd_publish_snapshot ( zb_uint8_t  param,
const zb_addr_u dst_addr,
zb_aps_addr_mode_t  dst_addr_mode,
zb_uint8_t  dst_ep,
zb_uint8_t  src_ep,
const zb_zcl_metering_publish_snapshot_payload_t pl,
zb_callback_t  cb 
)

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Function for send PublishSnapshot command. On receiver's side callback ZCL device callback ZB_ZCL_REGISTER_DEVICE_CB will be called with ZB_ZCL_METERING_PUBLISH_SNAPSHOT_CB_ID

Parameters
param- Reference to buffer.
dst_addr- Address of the device to send command to.
dst_addr_mode- Address mode for dst_addr.
dst_ep- Destination endpoint.
src_ep- Current endpoint.
pl- Packet payload (ref to zb_zcl_metering_publish_snapshot_payload_t).
cb- Callback which should be called when the ZCL stack receives APS ack.

§ zb_zcl_metering_send_cmd_request_fast_poll_mode()

void zb_zcl_metering_send_cmd_request_fast_poll_mode ( zb_uint8_t  param,
zb_addr_u dst_addr,
zb_aps_addr_mode_t  dst_addr_mode,
zb_uint8_t  dst_ep,
zb_uint8_t  src_ep,
zb_zcl_metering_request_fast_poll_mode_payload_t payload,
zb_callback_t  cb 
)

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Function for send RequestFastPollMode command. On receiver's side callback ZCL device callback ZB_ZCL_REGISTER_DEVICE_CB will be called with ZB_ZCL_METERING_REQUEST_FAST_POLL_MODE_CB_ID

Parameters
param- Reference to buffer.
dst_addr- Address of the device to send command to.
dst_addr_mode- Address mode for dst_addr.
dst_ep- Destination endpoint.
src_ep- Current endpoint.
payload- Packet payload (ref to zb_zcl_metering_request_fast_poll_mode_payload_t).
cb- Callback which should be called when the ZCL stack receives APS ack.

§ zb_zcl_metering_send_cmd_request_fast_poll_mode_response()

void zb_zcl_metering_send_cmd_request_fast_poll_mode_response ( zb_uint8_t  param,
const zb_addr_u dst_addr,
zb_aps_addr_mode_t  dst_addr_mode,
zb_uint8_t  dst_ep,
zb_uint8_t  src_ep,
const zb_zcl_metering_request_fast_poll_mode_response_payload_t pl,
zb_uint8_t  pl_size,
zb_uint8_t  tsn,
zb_callback_t  cb 
)

#include </home/developer/.conan/data/ti_zigbee/9.10.00.17/library-lprf/ga/build/f6d18801b7b469a709ae7e8290b03ecdc7a7ad4c/zboss_r23/include/zcl/zb_zcl_metering.h>

Function for send RequestFastPollMode command. On receiver's side callback ZCL device callback ZB_ZCL_REGISTER_DEVICE_CB will be called with ZB_ZCL_METERING_REQUEST_FAST_POLL_MODE_CB_ID

Parameters
param- Reference to buffer.
dst_addr- Address of the device to send command to.
dst_addr_mode- Address mode for dst_addr.
dst_ep- Destination endpoint.
src_ep- Current endpoint.
pl- Packet payload (ref to zb_zcl_metering_request_fast_poll_mode_response_payload_t).
pl_size- size in bytes of input payload. Stack can calculate actual payload size. Set pl_size to 0 for it.
tsn- transaction sequence number of response
cb- Callback which should be called when the ZCL stack receives APS ack.