TI BLE5-Stack API Documentation  9.11.00
Data Fields
gapLinkUpdateEvent_t Struct Reference

Data Fields

uint16_t connectionHandle
 Connection handle of the update.
 
uint16_t connInterval
 Requested connection interval.
 
uint16_t connLatency
 Requested connection latency.
 
uint16_t connTimeout
 Requested connection timeout.
 
osal_event_hdr_t hdr
 GAP_MSG_EVENT and status
 
uint8_t opcode
 GAP_LINK_PARAM_UPDATE_EVENT
 
uint8_t status
 status from link layer, defined in ll.h
 

Detailed Description

GAP_LINK_PARAM_UPDATE_EVENT message format.

This message is sent to the app when the connection parameters update request is complete.


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale