TI BLE5-Stack API Documentation  9.11.01
Data Fields
attHandleValueNoti_t Struct Reference

Handle Value Notification format. More...

Data Fields

uint16 handle
 Handle of the attribute that has been changed (must be first field) More...
 
uint16 len
 Length of value. More...
 
uint8 * pValue
 Current value of the attribute (0 to ATT_MTU_SIZE-3) More...
 

Detailed Description

Handle Value Notification format.

for method ATT_HANDLE_VALUE_NOTI

Field Documentation

§ handle

uint16 handle

Handle of the attribute that has been changed (must be first field)

§ len

uint16 len

Length of value.

§ pValue

uint8* pValue

Current value of the attribute (0 to ATT_MTU_SIZE-3)


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale