![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.11.01
|
Data Fields | |
| uint16_t | connectionHandle |
| connection Handle More... | |
| osal_event_hdr_t | hdr |
| GAP_MSG_EVENT and status More... | |
| uint8_t | opcode |
| GAP_PAIRING_REQ_EVENT More... | |
| gapPairingReq_t | pairReq |
| The Pairing Request fields received. More... | |
GAP_PAIRING_REQ_EVENT message format.
This message is sent when an unexpected Pairing Request is received and pairing must be initiated with GAP_Authenticate using the pairReq field received here
This event will be consumed by the gapbondmgr if it exists.
| uint16_t connectionHandle |
connection Handle
| osal_event_hdr_t hdr |
GAP_MSG_EVENT and status
| uint8_t opcode |
| gapPairingReq_t pairReq |
The Pairing Request fields received.