TI BLE5-Stack API Documentation  9.11.01
Data Fields
l2capFlowCtrlCredit_t Struct Reference

Flow Control Credit format. More...

Data Fields

uint16 CID
 Represents Source CID of device sending credit packet. More...
 
uint16 credits
 Number of LE-frames that can be sent to local device. More...
 

Detailed Description

Flow Control Credit format.

Field Documentation

§ CID

uint16 CID

Represents Source CID of device sending credit packet.

§ credits

uint16 credits

Number of LE-frames that can be sent to local device.


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale