Data Structures | Macros | Typedefs | Functions
Temperature.h File Reference

Detailed Description

Temperature driver.


Overview

The Temperature driver provides services related to measuring and reacting to the current temperature of the chip and changes to it.

The two main services provided are:

Usage

Initialisation

Unlike most drivers, there is only a single instance of the temperature driver that is always available once Temperature_init() is called. Temperature_init() should be called once before using other Temperature driver APIs. It is not called automatically via SysConfig generated code. Subsequent Temperature_init() calls will have no effect.

Getting the Current Temperature

The most basic function of the driver is to provide the current temperature and return it. It is encoded as a signed integer in degrees C.

Notifications

The other major function of the Temperature driver is to notify the application when the temperature changes and crosses an application-defined threshold.

There are three default usecases for this:

Registering Notifications

There are three functions that register a notification for the application:

Multiple notifications may be registered. The different parts of the application and drivers that need to respond to a temperature change do not need to know of one another. Each notification must have its own Temperature_NotifyObj and must be registered individually.

Notification Callbacks

Once the chip temperature crosses the smallest high threshold or largest low threshold amongst the registered notifications, the driver will iterate over the entire list of registered notification and check which ones have triggered. Notifications that have triggered are removed from the list of registered notifications and thus are no longer registered. Their callback function is then invoked.

If an application wishes to re-register a notification that just triggered and was unregistered, it may register it again from within the notification callback or another context.

It is possible to determine whether the high or low threshold triggered the notification callback as follows:

Unregistering Notifications

Registered notifications are unregistered in two ways:

Unregistered notifications may be registered again at any time.

Measured vs True Temperature

While the driver aims to supply and act on an accurate absolute temperature, there will be differences between the measured vs the true temperature due to inherent variances in the manufacturing process. The nature of these differences varies by device family.

Examples of such differences:

It is strongly recommended to read the device-specific Temperature driver documentation for details of the temperature sensor characteristics and how they might affect choices of threshold values.

Synopsis

#define WINDOW_DELTA 10
currentTemperature = Temperature_getTemperature();
result = Temperature_registerNotifyRange(&notifyObject,
currentTemperature + WINDOW_DELTA,
currentTemperature - WINDOW_DELTA,
myNotifyFxn,
clientArg);

Examples

Register a High Threshold Notification

// The notification will trigger when the temperature reaches 40 C
#define THRESHOLD_CUTOFF 40
void thresholdNotifyFxn(int16_t currentTemperature,
int16_t thresholdTemperature,
uintptr_t clientArg,
Temperature_NotifyObj *notifyObject) {
// Post a semaphore, set a flag, or otherwise act upon the temperature
// change.
}
...
// Initialize the Temperature driver and register a notification.
Temperature_init();
int_fast16_t status = Temperature_registerNotifyHigh(notifyObject,
THRESHOLD_CUTOFF,
thresholdNotifyFxn,
NULL);
// Handle error
}

Register a Range Threshold Notification and Re-register in Callback

#define THRESHOLD_DELTA 5
void deltaNotificationFxn(int16_t currentTemperature,
int16_t thresholdTemperature,
uintptr_t clientArg,
Temperature_NotifyObj *notifyObject) {
int_fast16_t status;
status = Temperature_registerNotifyRange(notifyObject,
currentTemperature + THRESHOLD_DELTA,
currentTemperature - THRESHOLD_DELTA,
deltaNotificationFxn,
NULL);
if (status != Temperature_STATUS_SUCCESS) {
while(1);
}
}
...
// Initialize the Temperature driver and register a notification.
Temperature_init();
int16_t currentTemperature = Temperature_getTemperature();
int_fast16_t status = Temperature_registerNotifyRange(notifyObject,
currentTemperature + THRESHOLD_DELTA,
currentTemperature - THRESHOLD_DELTA,
deltaNotificationFxn,
NULL);
#include <stdbool.h>
#include <stddef.h>
#include <stdint.h>
#include <ti/drivers/utils/List.h>
Include dependency graph for Temperature.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  Temperature_NotifyObj
 Temperature notify object structure. More...
 

Macros

#define Temperature_STATUS_RESERVED   (-32)
 
#define Temperature_STATUS_SUCCESS   (0)
 Successful status code. More...
 
#define Temperature_STATUS_ERROR   (-1)
 Generic error status code. More...
 

Typedefs

typedef void(* Temperature_NotifyFxn) (int16_t currentTemperature, int16_t thresholdTemperature, uintptr_t clientArg, Temperature_NotifyObj *notifyObject)
 Function prototype for a notification callback. More...
 

Functions

void Temperature_init (void)
 This function initializes the Temperature driver. More...
 
int16_t Temperature_getTemperature (void)
 Gets the current temperature in degrees C. More...
 
int_fast16_t Temperature_registerNotifyHigh (Temperature_NotifyObj *notifyObject, int16_t thresholdHigh, Temperature_NotifyFxn notifyFxn, uintptr_t clientArg)
 Registers a notification with a high threshold. More...
 
int_fast16_t Temperature_registerNotifyLow (Temperature_NotifyObj *notifyObject, int16_t thresholdLow, Temperature_NotifyFxn notifyFxn, uintptr_t clientArg)
 Registers a notification with a low threshold. More...
 
int_fast16_t Temperature_registerNotifyRange (Temperature_NotifyObj *notifyObject, int16_t thresholdHigh, int16_t thresholdLow, Temperature_NotifyFxn notifyFxn, uintptr_t clientArg)
 Registers a notification with both a high and low threshold. More...
 
int_fast16_t Temperature_unregisterNotify (Temperature_NotifyObj *notifyObject)
 Unregisters a currently registered notification. More...
 
int16_t Temperature_getThresholdHigh (Temperature_NotifyObj *notifyObject)
 Get the high threshold of a notification. More...
 
int16_t Temperature_getThresholdLow (Temperature_NotifyObj *notifyObject)
 Get the low threshold of a notification. More...
 
void Temperature_getThresholdRange (Temperature_NotifyObj *notifyObject, int16_t *thresholdHigh, int16_t *thresholdLow)
 Get the high and low threshold of a notification. More...
 
uintptr_t Temperature_getClientArg (Temperature_NotifyObj *notifyObject)
 Get the application-provided clientArg of a notification. More...
 
Temperature_NotifyFxn Temperature_getNotifyFxn (Temperature_NotifyObj *notifyObject)
 Get the notifyFxn provided during registration. More...
 

Macro Definition Documentation

§ Temperature_STATUS_RESERVED

#define Temperature_STATUS_RESERVED   (-32)

Common Temperature status code reservation offset. Temperature driver implementations should offset status codes with Temperature_STATUS_RESERVED growing negatively.

Example implementation specific status codes:

#define TemperatureXYZ_STATUS_ERROR0 Temperature_STATUS_RESERVED - 0
#define TemperatureXYZ_STATUS_ERROR1 Temperature_STATUS_RESERVED - 1
#define TemperatureXYZ_STATUS_ERROR2 Temperature_STATUS_RESERVED - 2

§ Temperature_STATUS_SUCCESS

#define Temperature_STATUS_SUCCESS   (0)

Successful status code.

Functions return Temperature_STATUS_SUCCESS if the function was executed successfully.

§ Temperature_STATUS_ERROR

#define Temperature_STATUS_ERROR   (-1)

Generic error status code.

Functions return Temperature_STATUS_ERROR if the function was not executed successfully.

Typedef Documentation

§ Temperature_NotifyFxn

typedef void(* Temperature_NotifyFxn) (int16_t currentTemperature, int16_t thresholdTemperature, uintptr_t clientArg, Temperature_NotifyObj *notifyObject)

Function prototype for a notification callback.

Parameters
[in]currentTemperatureCurrent chip temperature
[in]thresholdTemperatureTemperature threshold that caused this notification callback.
[in]clientArgArgument provided by the application during registration.
[in/out]notifyObject The notification object that was registered previously. This pointer may be used to register the notification again with updated inputs from within the notification callback.

Function Documentation

§ Temperature_init()

void Temperature_init ( void  )

This function initializes the Temperature driver.

This function initializes the internal state of the Temperature driver. It must be called before calling any other Temperature functions. Calling this function multiple times will only have an effect the first time.

Note
This function should be called manually before using the temperature API. It will not be called automatically via SysConfig generated code.

§ Temperature_getTemperature()

int16_t Temperature_getTemperature ( void  )

Gets the current temperature in degrees C.

Returns
Current temperature in degrees C

§ Temperature_registerNotifyHigh()

int_fast16_t Temperature_registerNotifyHigh ( Temperature_NotifyObj notifyObject,
int16_t  thresholdHigh,
Temperature_NotifyFxn  notifyFxn,
uintptr_t  clientArg 
)

Registers a notification with a high threshold.

This function registers a Temperature notification with a high threshold. Once the chip temperature rises above thresholdHigh, notifyFxn is called and the notification is automatically unregistered.

Parameters
notifyObjectStructure to be initialized. After returning, it will contain the data necessary to issue a notification callback. The memory of the structure must persist while the notification is registered.
[in]thresholdHighThreshold temperature in degrees C
[in]notifyFxnCallback function that is called once the chip temperature rises above thresholdHigh.
[in]clientArgApplication-specified argument
Return values
Temperature_STATUS_SUCCESSThe notification was successfully registered.
Temperature_STATUS_ERRORThere was an error during registration.
Precondition
Temperature_init() called

§ Temperature_registerNotifyLow()

int_fast16_t Temperature_registerNotifyLow ( Temperature_NotifyObj notifyObject,
int16_t  thresholdLow,
Temperature_NotifyFxn  notifyFxn,
uintptr_t  clientArg 
)

Registers a notification with a low threshold.

This function registers a Temperature notification with a low threshold. Once the chip temperature falls below thresholdLow, notifyFxn is called and the notification is automatically unregistered.

Parameters
notifyObjectStructure to be initialized. After returning, it will contain the data necessary to issue a notification callback. The memory of the structure must persist while the notification is registered.
[in]thresholdLowThreshold temperature in degrees C
[in]notifyFxnCallback function that is called once the chip temperature falls below thresholdLow.
[in]clientArgApplication-specified argument
Return values
Temperature_STATUS_SUCCESSThe notification was successfully registered.
Temperature_STATUS_ERRORThere was an error during registration.
Precondition
Temperature_init() called

§ Temperature_registerNotifyRange()

int_fast16_t Temperature_registerNotifyRange ( Temperature_NotifyObj notifyObject,
int16_t  thresholdHigh,
int16_t  thresholdLow,
Temperature_NotifyFxn  notifyFxn,
uintptr_t  clientArg 
)

Registers a notification with both a high and low threshold.

This function registers a Temperature notification with a high and low threshold. Once the chip temperature rises above thresholdHigh or falls below thresholdLow, notifyFxn is called and the notification is automatically unregistered.

Parameters
notifyObjectStructure to be initialized. After returning, it will contain the data necessary to issue a notification callback. The memory of the structure must persist while the notification is registered.
[in]thresholdHighHigh threshold temperature in degrees C
[in]thresholdLowLow threshold temperature in degrees C
[in]notifyFxnCallback function that is called once the chip temperature falls below thresholdLow, or rises above thresholdHigh.
[in]clientArgApplication-specified argument
Return values
Temperature_STATUS_SUCCESSThe notification was successfully registered
Temperature_STATUS_ERRORThere was an error during registration
Precondition
Temperature_init() called

§ Temperature_unregisterNotify()

int_fast16_t Temperature_unregisterNotify ( Temperature_NotifyObj notifyObject)

Unregisters a currently registered notification.

This function unregisters a currently registered notification. It should not be called on a notifyObject that is not currently registered.

Parameters
notifyObjectNotification to unregister.
Return values
Temperature_STATUS_SUCCESSThe notification was successfully unregistered.
Temperature_STATUS_ERRORThere was an error during unregistration.
Precondition
Register notifyObject with Temperature_registerNotifyHigh(), Temperature_registerNotifyLow(), or Temperature_registerNotifyRange()

§ Temperature_getThresholdHigh()

int16_t Temperature_getThresholdHigh ( Temperature_NotifyObj notifyObject)

Get the high threshold of a notification.

This function should not be called on a notifyObject registered with Temperature_registerNotifyLow(). The high threshold value returned in that case will be a device-specific invalid temperature.

Parameters
notifyObjectNotification to get the high threshold of.
Returns
High threshold in degrees C.
Precondition
Register notifyObject with Temperature_registerNotifyHigh(), or Temperature_registerNotifyRange()

§ Temperature_getThresholdLow()

int16_t Temperature_getThresholdLow ( Temperature_NotifyObj notifyObject)

Get the low threshold of a notification.

This function should not be called on a notifyObject registered with Temperature_registerNotifyHigh(). The low threshold value returned in that case will be a device-specific invalid temperature.

Parameters
notifyObjectNotification to get the low threshold of.
Returns
Low threshold in degrees C.
Precondition
Register notifyObject with Temperature_registerNotifyLow(), or Temperature_registerNotifyRange()

§ Temperature_getThresholdRange()

void Temperature_getThresholdRange ( Temperature_NotifyObj notifyObject,
int16_t *  thresholdHigh,
int16_t *  thresholdLow 
)

Get the high and low threshold of a notification.

This function should not be called on a notifyObject registered with Temperature_registerNotifyLow() or Temperature_registerNotifyHigh(). The unconfigured threshold value returned in that case will be a device-specific invalid temperature.

Parameters
notifyObjectNotification to get the high and low threshold of.
[out]thresholdHighHigh threshold value in degrees C written back by this function.
[out]thresholdLowLow threshold value in degrees C written back by this function.
Precondition
Register notifyObject with Temperature_registerNotifyRange()

§ Temperature_getClientArg()

uintptr_t Temperature_getClientArg ( Temperature_NotifyObj notifyObject)

Get the application-provided clientArg of a notification.

Parameters
notifyObjectNotification to get the clientArg of.
Returns
The clientArg provided during registration.
Precondition
Register notifyObject with Temperature_registerNotifyHigh(), Temperature_registerNotifyLow(), or Temperature_registerNotifyRange()

§ Temperature_getNotifyFxn()

Temperature_NotifyFxn Temperature_getNotifyFxn ( Temperature_NotifyObj notifyObject)

Get the notifyFxn provided during registration.

Parameters
notifyObjectNotification to get the notifyFxn of.
Returns
The notifyFxn provided during registration
Precondition
Register notifyObject with Temperature_registerNotifyHigh(), Temperature_registerNotifyLow(), or Temperature_registerNotifyRange()
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale